Device Firmware Upgrade (DFU) over USB on LPC54114

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device Firmware Upgrade (DFU) over USB on LPC54114

ソリューションへジャンプ
2,291件の閲覧回数
Haider_Ali
Contributor II

Hello, I'm new to NXP controllers and need help in knowing if LPC54114 supports upgrade of flash via USB using DFU class?

In the datasheet, for ISP modes only USB mass storage device class (MSC) is mentioned.

Haider_Ali_0-1710874666276.pngHaider_Ali_0-1710874666276.png

Where as in USB section it says that it support DFU.

Haider_Ali_1-1710874794076.pngHaider_Ali_1-1710874794076.png

Appreciate if can share any example or where to get further information on above.

Is there any utility or software which can be used to upgrade the firmware?

thank you

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,254件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Haider_Ali 

1)Table 2 ISP mode means:

If use ISP mode to update firmware, supports USB mass storage device class ( MSC) mode.  Not supports USB DFU.

2) 34.2 &34.3 (in your screenshot ) means:

USB driver in  iLPC54114 ROM can implements DFU. If you want to use DFU update firmware, can write application based on the USB driver. For ISP mode update firmware, no need add application code.

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,255件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Haider_Ali 

1)Table 2 ISP mode means:

If use ISP mode to update firmware, supports USB mass storage device class ( MSC) mode.  Not supports USB DFU.

2) 34.2 &34.3 (in your screenshot ) means:

USB driver in  iLPC54114 ROM can implements DFU. If you want to use DFU update firmware, can write application based on the USB driver. For ISP mode update firmware, no need add application code.

 

BR

Alice

0 件の賞賛
返信
2,218件の閲覧回数
Haider_Ali
Contributor II

Thank you.

Regarding DFU update firmware, is there any example code or library to implement it?

0 件の賞賛
返信