Deep sleep and wake up using RTC in LPC54018

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Deep sleep and wake up using RTC in LPC54018

Jump to solution
4,309 Views
mitchkapa
Contributor III

Hello, I am essentially trying to replicate the success of this post (https://community.nxp.com/t5/LPC-Microcontrollers/Deep-sleep-and-wake-up-using-RTC-in-LPC54618/m-p/9...) but using the LPC54018 processor instead.  I placed a comment within that thread noting that I can see a wakeup occurring via the RTC however I cannot get execution to return to the main function.  Is there some fundamental difference between the LPC54618 and LPC54018 when using the RTC for deep sleep?

0 Kudos
Reply
1 Solution
4,263 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls try to use the line:

#define APP_EXCLUDE_FROM_DEEPSLEEP \

(SYSCON_PDRUNCFG_PDEN_SRAMX_MASK | SYSCON_PDRUNCFG_PDEN_SRAM0_MASK | SYSCON_PDRUNCFG_PDEN_SRAM1_2_3_MASK | \

SYSCON_PDRUNCFG_PDEN_VD6_MASK|SYSCON_PDRUNCFG_PDEN_WDT_OSC_MASK)

 

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
6 Replies
4,292 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the waking-up from deep-sleep follows up the interrupt procedure, in other words, when the waking-up happens, it enters ISR  firstly, after executing the ISR, it returns to main from ISR.

So you have to enable the alarm interrupt and create an ISR for the RTC alarm interrupt.

Pls have a try.

If you have issue, pls post your code, I will have a review.

BR

XiangJun Rong

 

0 Kudos
Reply
4,287 Views
mitchkapa
Contributor III

Below is the source code.  I am running this code on the LPCXpresso54018 development board.  Within the RTC_IRQHandler function I put multiple PRINTF statements and those do print so the wake up from sleep is happening.  But the "Alarm Occurs" message from the main body never prints.  Here is an example of the debug output:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
5
currSecond =: 1419534002Alarm will occur at: 2014-12-25 19: 0: 7

Interrupt occurs !!!!
I cleared the alarm flag !!!!
I got past the IF errata statement !!!!

_______________________________________________________

Here is the source code:

#include "fsl_debug_console.h"
#include "board.h"
#include "fsl_rtc.h"
#include "pin_mux.h"
#include <stdbool.h>
#include "peripherals.h"
#include "fsl_common.h"
#include "fsl_power.h"
 
 
/*******************************************************************************
* Definitions
******************************************************************************/
 
#define APP_EXCLUDE_FROM_DEEPSLEEP \
(SYSCON_PDRUNCFG_PDEN_SRAMX_MASK | SYSCON_PDRUNCFG_PDEN_SRAM0_MASK | SYSCON_PDRUNCFG_PDEN_SRAM1_2_3_MASK | SYSCON_PDRUNCFG_PDEN_WDT_OSC_MASK \
)
/*******************************************************************************
* Prototypes
******************************************************************************/
 
/*******************************************************************************
* Variables
******************************************************************************/
 
volatile bool busyWait;
 
/*******************************************************************************
* Code
******************************************************************************/
 
/*!
* @brief ISR for Alarm interrupt
*
* This function changes the state of busyWait.
*/
void RTC_IRQHandler(void)
{
if (RTC_GetStatusFlags(RTC) & kRTC_AlarmFlag)
{
PRINTF("\r\n Interrupt occurs !!!! ");
busyWait = false;
 
/* Clear alarm flag */
RTC_ClearStatusFlags(RTC, kRTC_AlarmFlag);
PRINTF("\r\n I cleared the alarm flag !!!! ");
 
}
/* Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F Store immediate overlapping
exception return operation might vector to incorrect interrupt */
#if defined __CORTEX_M && (__CORTEX_M == 4U)
__DSB();
#endif
PRINTF("\r\n I got past the IF errata statement !!!! ");
 
}
 
/*!
* @brief Main function
*/
int main(void)
{
gpio_pin_config_t led_config = {kGPIO_DigitalOutput, 0,};
uint32_t sec;
uint32_t currSeconds;
uint8_t index;
rtc_datetime_t date;
 
/* Board pin, clock, debug console init */
/* attach 12 MHz clock to FLEXCOMM0 (debug console) */
CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);
 
/* Enable the RTC 32K Oscillator */
SYSCON->RTCOSCCTRL |= SYSCON_RTCOSCCTRL_EN_MASK;
 
BOARD_InitPins();
BOARD_BootClockFROHF48M();
BOARD_InitDebugConsole();
CLOCK_EnableClock(kCLOCK_Gpio3);
/* Init RTC */
RTC_Init(RTC);
 
PRINTF("RTC example: set up time to wake up an alarm\r\n");
 
/* Set a start date time and start RT */
date.year = 2014U;
date.month = 12U;
date.day = 25U;
date.hour = 19U;
date.minute = 0;
date.second = 0;
 
/* RTC time counter has to be stopped before setting the date & time in the TSR register */
RTC_StopTimer(RTC);
 
/* Set RTC time to default */
RTC_SetDatetime(RTC, &date);
 
/* Enable RTC alarm interrupt */
RTC_EnableInterrupts(RTC, kRTC_AlarmInterruptEnable);
 
/* Enable at the NVIC */
EnableIRQ(RTC_IRQn);
EnableDeepSleepIRQ(RTC_IRQn);
/* Start the RTC time counter */
RTC_StartTimer(RTC);
 
/* This loop will set the RTC alarm */
while (1)
{
busyWait = true;
index = 0;
sec = 0;
/* Get date time */
RTC_GetDatetime(RTC, &date);
 
/* print default time */
PRINTF("Current datetime: %04d-%02d-%02d %02d:%02d:%02d\r\n",
date.year,
date.month,
date.day,
date.hour,
date.minute,
date.second);
 
/* Get alarm time from user */
PRINTF("Please input the number of second to wait for alarm \r\n");
PRINTF("The second must be positive value\r\n");
while (index != 0x0D)
{
index = GETCHAR();
if((index >= '0') && (index <= '9'))
{
PUTCHAR(index);
sec = sec * 10 + (index - 0x30U);
}
}
PRINTF("\r\n");
 
/* Read the RTC seconds register to get current time in seconds */
currSeconds = RTC->COUNT;
PRINTF("currSecond =: %d", currSeconds);
 
/* Add alarm seconds to current time */
currSeconds += sec;
 
/* Set alarm time in seconds */
RTC->MATCH = currSeconds;
//RTC_SetAlarm(RTC, currSeconds);
 
/* Get alarm time */
RTC_GetAlarm(RTC, &date);
 
/* Print alarm time */
PRINTF("Alarm will occur at: %04d-%02d-%02d %02d:%02d:%02d\r\n",
date.year,
date.month,
date.day,
date.hour,
date.minute,
date.second);
POWER_EnterDeepSleep(APP_EXCLUDE_FROM_DEEPSLEEP);
//POWER_EnterSleep();
/* Wait until alarm occurs */
while (busyWait)
{
}
 
PRINTF("\r\n Alarm occurs !!!! ");
}
}

 

0 Kudos
Reply
4,274 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

where you declare the bool variable busyWait?

How about  commenting the following line

while (busyWait)
{
}

BR

XiangJun Rong

0 Kudos
Reply
4,268 Views
mitchkapa
Contributor III

The variable is declared here:

/*******************************************************************************
* Variables
******************************************************************************/
 
volatile bool busyWait;
 
I tried commenting out the while loop and the code still does not reach the final PRINTF statement.
0 Kudos
Reply
4,264 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls try to use the line:

#define APP_EXCLUDE_FROM_DEEPSLEEP \

(SYSCON_PDRUNCFG_PDEN_SRAMX_MASK | SYSCON_PDRUNCFG_PDEN_SRAM0_MASK | SYSCON_PDRUNCFG_PDEN_SRAM1_2_3_MASK | \

SYSCON_PDRUNCFG_PDEN_VD6_MASK|SYSCON_PDRUNCFG_PDEN_WDT_OSC_MASK)

 

BR

XiangJun Rong

0 Kudos
Reply
4,258 Views
mitchkapa
Contributor III

Thank you this was the solution I was missing SYSCON_PDRUNCFG_PDEN_VD6_MASK from the exclusions.

0 Kudos
Reply