Deep power down mode LPC802 supply current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Deep power down mode LPC802 supply current

6,440件の閲覧回数
eva
Contributor II

I am using a LPC802 in deep power down mode, the current should be 0.15uA, but I have a 13,8uA current consumption.

Following the example "power_mode_switch_lpc.c":

I configure the wakeup pin:

POWER_DeepPowerDownWakeupSourceSelect(kPmu_Dpd_En_Pio0_17);

where:

static inline void POWER_DeepPowerDownWakeupSourceSelect(uint32_t wakeup_pin)
{
PMU->WUENAREG |= wakeup_pin;
}

and to enter deep power down mode call the function:

POWER_EnterDeepPowerDownMode();

where:

void POWER_EnterDeepPowerDownMode(void)
{
uint32_t pmsk;

pmsk = __get_PRIMASK();
__disable_irq();

/* make sure NODPD is cleared */
PMU->PCON = (PMU->PCON & (~(PMU_PCON_PM_MASK | PMU_PCON_NODPD_MASK))) | PMU_PCON_PM(kPmu_Deep_PowerDown);


/* enable Deepsleep mode in the ARM-CORTEX M0+ SCR register */
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;

/*clear wake up pin status flag*/
PMU->WUSRCREG |= PMU_WUSRCREG_WUSRCREG_MASK;

/* Enter powerdown mode */
__WFI();

/* disable Deepsleep mode in the ARM-CORTEX M0+ SCR register */
SCB->SCR &= ~SCB_SCR_SLEEPDEEP_Msk;
__set_PRIMASK(pmsk);
}

All the pins are without external connections, except wakeup pin, where I have an external pullup

0 件の賞賛
返信
14 返答(返信)

6,029件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I asked for get more details because in my department does not have that board, the engineer that help me have these comments.... I have tested the customer's code in LPC802 EVK, according to my test results the power consumption when deep power down is 0.18uA. Just changed the wakeup pin from P0_17 to P0_8 based on LPC802 EVK.

I doubt this issue was caused by customer's board, suggest try to change the WAKEUP pin to test this issue.

Best regards,
Pavel

0 件の賞賛
返信

5,827件の閲覧回数
eva
Contributor II

Thank you Pavel. Which is the value of the pullup resistance you have in your wakeup pin?

Best regards,

Eva

0 件の賞賛
返信

5,816件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, they mentioned P0_8 based on LPC802 EVK.

Pavel_Hernandez_0-1716821506318.png

Best regards,
Pavel

 

0 件の賞賛
返信

6,193件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I suggest removing the 56k RPUL. To test this issue

Pavel_Hernandez_0-1715702802343.png

Best regards,
Pavel

0 件の賞賛
返信

6,186件の閲覧回数
eva
Contributor II

Hello, if I remove 56k pullup, current consumption increases up to 45 uA

6,093件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I have checked the code, suggest mode the below configuration to test this issue.

Do not disable the GPIO0 clock,

Pavel_Hernandez_0-1716233992519.png

Because I don't have your board, it's limited for me to check this issue.

Best regards,
Pavel

0 件の賞賛
返信

6,050件の閲覧回数
eva
Contributor II

Hello Pavel,

I tried your suggestion, but the result is the same. I have the same current consumtion either I call LP_PreEnterLowPower function or not.

In Deep power down mode, power is shut off to entire chip except for the WAKEUP pins, digital peripherals are off, and PIOn_m pins are Floating, so that makes sense.

I could think that I have a problem in PCB, but if I enter power down mode instead of Deep power down mode, the current consumption goes to 6uA, that is the value in datasheet. So that makes me think that something is wrong in software.

I have measured current through pullup resistor, it is 0,4uA aprox, so it seems that 13uA consumption is internal.

Best regads

6,182件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, let me get more information.

Best regards,
Pavel

0 件の賞賛
返信

6,340件の閲覧回数
eva
Contributor II

Hello Pavel,

I am using a custom board, all the pins are disconnected except the wake up pin (it has an external pullup resistor of 56komhs), and VDD is 3v3.

I am using a polimeter in series with VDD to measure the current. If I write value 0x02 in PMU->PCON PM bits(power down mode) instead of value 0x03 (deep power down mode), I measure a current of 6uA (same as datasheet).

The temperature is 22ºC.

Regarding pins I tryed floating pins and also with all pins configured as GPIO outputs driven LOW and pull-up resistors disabled, but result is the same.  User manual says:"All functional pins are tri-stated in deep power-down mode except for the WAKEUP pin".

The debugger is disconnected from the board.

Best regards,

Eva

0 件の賞賛
返信

6,421件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, let me get into your case when I have more information I will contact you.

Best regards,
Pavel

0 件の賞賛
返信

6,378件の閲覧回数
eva
Contributor II

Hello Pavel, any news regarding this issue? 6uA is too much for my application, I would need a current consuption below 1uA. 

Thank you in advance.

0 件の賞賛
返信

6,410件の閲覧回数
eva
Contributor II

Thank you Pavel.

If I write value 0x02 in PMU->PCON PM bits using the same function, the current consumption goes to 6,5uA (power down mode)

With 0x03 value (deep power down mode), consumption is 13,8uA

0 件の賞賛
返信

6,372件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, sorry for the late response, I´m following your case, I have some questions about it.

Could you let me know if you are using a EVK or custom board?
Could you share a schematic about how you are made the measure?

The table on it has this note.
[1] Typical ratings are not guaranteed. The values listed are for room temperature (25 C), VDD = 3.3 V.

What kind of temperature do you have?
See the Fig 19. Deep power-down mode.

Did you put floating the unused pins?
[3] IDD measurements were performed with all pins configured as GPIO outputs driven LOW and pull-up resistors disabled. 

In addition, please make sure you DISCONNECT the board with IDE debugger when measure. 

Best regards,
Pavel

0 件の賞賛
返信

6,333件の閲覧回数
eva
Contributor II

Hello Pavel,

I am using a custom board, all the pins are disconnected except the wake up pin (it has an external pullup resistor of 56komhs), and VDD is 3v3.

I am using a polimeter in series with VDD to measure the current. If I write value 0x02 in PMU->PCON PM bits(power down mode) instead of value 0x03 (deep power down mode), I measure a current of 6uA (same as datasheet).

The temperature is 22ºC.

Regarding pins I tryed floating pins and also with all pins configured as GPIO outputs driven LOW and pull-up resistors disabled, but result is the same.  User manual says:"All functional pins are tri-stated in deep power-down mode except for the WAKEUP pin".

The debugger is disconnected from the board.

Best regards,

Eva

0 件の賞賛
返信