Debugging problems when changing RAM order/size (LPCXpresso 54628)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging problems when changing RAM order/size (LPCXpresso 54628)

1,499件の閲覧回数
SimonSchnee
Contributor III

Hello!

 

I currently struggle to get my application running and debug it on my LPCXpresso board 54628.

As you can see in the screenshots, after building my project with the default memory settings that the whole application does not fit into the first RAM location (SRAM_UPPER).

Building-Error_Not-Enough-Space.PNG

 

Therefore I wanted to increase the memory or change the memory order, for example I would use the BOARD-SRAM memory space which would have enough space for the application.

Building-Successful_Enough-Memory.PNG

 

But when I build it and want to debug it, debugging with LinkServer does not work and I get the following error:

Debug-Error.jpgDebug-Error_2.PNG

 

I am currently using MCUXpresso v11.4.1 and the appropriate SDK v12.10.0.

Would be nice if someone can help me here.

 

Best regards!

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,462件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @SimonSchnee,

This case is being followed in your internal ticket.

Best regards, Raul.

0 件の賞賛
返信