Debugger stack required

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger stack required

1,730件の閲覧回数
TEMCEFF
Contributor IV

As an embedded developer we need more debuggers. So we are trying to develop LPC-Link2 debugger(we are using this now). We found hardware in internet. Hardware we will prepare. We need stack (firmware). Is there any possibility to get debugger stack from NXP people?

0 件の賞賛
返信
2 返答(返信)

1,523件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

Hi Anusha,

We don't provide source code for the LPC-Link2 firmware that is developed by NXP for LPCXpresso/MCUXpresso/LPCScrypt. However, if you copy the circuitry used on the LPCXpresso V2/V3 boards then you should be able to use the firmware as-is, using LPCScrypt. Note that we cant help debug any issues with a hardware development like this.

If lower performance is OK then you can copy the LPC11U3x-based debug probe used on LPCXpresso MAX boards. These boards use the mbed CMSIS-DAP debug probe software, and the source for that is available on the mbed developers' site. FYI, ARM also released source for an implementation of CMSIS-DAP on the LPC4322 on this site; see:

https://github.com/mbedmicro/DAPLink, although we cannot guarantee this will work with LPCXpresso/MCUXpresso IDEs.

Regards,

Brendon

0 件の賞賛
返信

1,523件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Anusha G,

To provide the fastest possible support I want to point you to a similar question which has been answered on our NXP community.

Please refer to http://www.nxp.com/assets/documents/data/en/supporting-information/Debug_Probe_Firmware_Programming.... to view the details.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信