Debug out problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug out problem

3,932 次查看
dimitrissideris
Contributor III

Hi there,

I am running the lpc open examples and many of these examples are using debugout functions to print messages.

In board.c i have enabled (this is the dafault configuration) #include "retarget.h".

The debugout messages were displayed in serial terminal at COM3 fine.

Suddenly no messages are displayed. The weird thing is that when i press keys in keyboard i can handle it properily.

It seems that debug in works properly but debug out not.

I am in a middle of a delivery so if any has any advice or idea please help!

Thanx a lot!

0 项奖励
回复
7 回复数

3,510 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

User has created new thread : https://community.nxp.com/thread/434445 

0 项奖励
回复

3,510 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Dimitris Sideris,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

Before answer the question, I was wondering if you can tell me what the board and the version of the LPCOpen you use.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,510 次查看
dimitrissideris
Contributor III

Hi again jeremyzhou,

my board is lpcxpresso4367 and lpcopen version 2.19 (the latest).

The weird thing is as i mentioned before that i never had a problem with the debugout messages.

The only thing that it might affected is that i installed a driver for an oscilloscope to pc and i had to install also some additional usb drives from National Instruments.

Now i have uninstalled them and reinstalled the LPC-LinkII Ucom Port driver.

My project libraries are redlib (nohost) and not using semihosting.

Hope that the above info helps.

0 项奖励
回复

3,510 次查看
dimitrissideris
Contributor III

I am trying to fix this so i restored windows to a previous state before the potential messing with the usb drivers.

I also downloaded lpcxpresso IDE 8.2.0.

Still have the same problem.

I can debug correctly, if i choose blindly the options from serial terminal debugin takes it as input but NO debugout messages are printed.

Plz help!

0 项奖励
回复

3,510 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.

I'd like to suggest that you can debug the board with a new PC or use the P4 FTDI header to connect the PC with the TTL-232R-3V3 cable.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,510 次查看
dimitrissideris
Contributor III

What do you think is the problem?

Either a new pc or buying sth in not an option unfortunately!

0 项奖励
回复

3,510 次查看
dimitrissideris
Contributor III

I could really use some help.

Most lpcopen examples need a terminal input so without debugout messages i practically cannot use uC.

0 项奖励
回复