Debug in _WFI mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug in _WFI mode?

5,718 Views
himanshudoshi
Contributor III

Hello to all,

I am trying to see, what's happening to the program inside the _WFI() mode, but when I try to do so in debug mode. It doesn't proceed further and forcefully we need to stop the debug operation. Does any body know how to deal with such a small issue??

Thanking you, 

-Regards,

Himanshu Doshi

Labels (4)
Tags (1)
7 Replies

5,168 Views
lpcxpresso_supp
NXP Employee
NXP Employee

When the cpu encounters a WFI instruction, it basically goes into a simple low power mode, and will no longer execute any instructions until an interrupt is triggered, at which point it will wake up again and enter the appropriate interrupt handler. Thus whilst in WFI "mode", waiting for an interrupt to happen, your application has basically stopped executing.

From a debug point of view, depending on your debug tools, it is possible that your debugger might actually time out the debug connection whilst the cpu is in WFI "mode" if an interrupt is not triggered within a certain timeframe. But in most cases, your system will probably have at least one interrupt triggering on a regular enough basis (such as Systick, or another timer), for the WFI to effectively be "invisible" from the debug point of view.

Regards,

MCUXpresso IDE Support

5,168 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Himanshu Doshi,

The execution of the WFI instruction will cause immediate entry to the sleep or deep sleep power modes, no more code is executed after this instruction. Sleep mode is exited automatically when an interrupt enabled by the NVIC arrives at the processor or a reset occurs. Please see the User Manual for details on which interrupt sources are connected to NVIC.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

5,168 Views
himanshudoshi
Contributor III

Hello, Mr. Mendoza

Thank you very much for your reply. I am using SysTick_Handler to get the interrupt in WFI (sleep mode). And, there is a piece of code written in the SysTick_Handler. Can you suggest me how should I debug the code inside the SysTick???

The piece of code looks like this:

void SysTick_Handler(void)
{
asm(
"STR.W R3,[R7]\t\n"
"STR.W R4,[R3]\t\n"
"STR.W R5,[R4]\t\n"

);
}

Thanking you once again,

Regards,

Himanshu

0 Kudos
Reply

5,168 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Himanshu,

 

Are you able to set a breakpoint inside the systick handler? If the debug connection gets lost because of the low power mode being used you could try attaching to the system as explained to Simon.


Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

5,168 Views
himanshudoshi
Contributor III

Hello Carlos Mendoza,

 

Thank you very much for your reply. As suggested by you, I have provided a toggle break point into the _WFI program, but while debugging, an error was flashing at the bottom of IDE: "Stalled on bus operation". I have restarted the IDE and try again but it's the same and also the same thing happened on the debugger configuration to make attach only option true. Can you comment on it??

How to debug a program in the _WFI mode??

Regards,

Himanshu 

0 Kudos
Reply

5,168 Views
simonwyss
Contributor III

According to the user manual UM10805 Page 80 it is NOT possible to debug the low-power modes. (http://www.nxp.com/docs/en/user-guide/UM10850.pdf )

pastedImage_12.png

But in the appnote AN11611 is written that the debugger can be reconnected. However, NXP doesn't write in the appnote, how the reconnection could be accomplished.

pastedImage_13.png

NXP, can you give use some advice? 

I also like to know, how I can restart the debugger if I had previous finished the debug session and the code has not changed until now (no recompilation and flashing required).

0 Kudos
Reply

5,168 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Simon,

You should use the "Attach Only" option in the debug configurations, this will allow you to debug a running system:

https://community.nxp.com/message/630604 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer