Dear NXP Support please check SWIM download link is dead

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dear NXP Support please check SWIM download link is dead

2,940件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by studyembedded on Thu Mar 05 07:27:51 MST 2015
Hi NXP,
The following link for downloading SWIM is dead, please provide us the alternate download link.

SWIM Download

Thanks!!
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,655件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Mar 05 08:12:46 MST 2015
Hi,
Check it at
http://www.lpcware.com/content/nxpfile/an10815-swim-nxps-basic-graphics-library-lpc-products-v30
0 件の賞賛
返信

2,655件の閲覧回数
some1inct
Contributor I

That link no longer provides access to SWIM

0 件の賞賛
返信

2,655件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Attached is the AN10815.
Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,655件の閲覧回数
some1inct
Contributor I

Thank you, but I was trying to check if there had been any updates. There were two updates since the application note that you posted. I have rev 3 including the code.

Rev   Date   Description
3   20110615   Added support for EA LPC1788 OEM board.
2   20110501   Added support for Hitex LPC1850.
1   20090501   Initial revision.

0 件の賞賛
返信