Deadtime in lpc1768

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Deadtime in lpc1768

1,434 Views
gaviprakash
Contributor I

Hi,

Iam generating MCPWM with deadtime in LPC1768.but iam not able to generate dead time I read datasheet but it is not generating can anyone please help.below is my code

main()

{

SystemInit();                    //Clock and PLL configuration 
 
  LPC_SC->PCONP |= (1<<17); /* Power ON Timer0,1 */
  LPC_SC->PCLKSEL1 |=(1<<30)|(1<<31);
  LPC_PINCON->PINSEL3 |= (1<<12)|(1<<6);
  LPC_PINCON->PINMODE3 |= (1<<6)|(1<<7)|(1<<12)|(1<<13);
      LPC_GPIO1->FIODIR |= (1<<19)|(1<<22);
   LPC_MCPWM->MCCCP = (1<<0)|(1<<1)|(1<<2)|(1<<3);
   LPC_MCPWM->MCCON_SET |=(1<<3)|(1<<31)|(1<<29);//|(1<<1)|(1<<9) ;
  LPC_MCPWM->MCTIM0 = 0;
    LPC_MCPWM->MCPER0 = 1000;
  LPC_MCPWM->MCPW0 = 600;
  LPC_MCPWM->MCDEADTIME = 0x100 ;
  for(i=0;i<10000;i++)
  for(j=0;j<1000;j++);
  LPC_MCPWM->MCCON_SET |= (1<<0);
     while(1)
     { 
    
     }
 }

Thanks

0 Kudos
Reply
1 Reply

1,221 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi gavi,

Is it working correctly without the dead time insertion?

I have reviewed the code snippet above and it seems to be correctly configured. You could also try using the LPC175x_6x CMSIS-Compliant Standard Peripheral Firmware Driver as reference for your application, it comes with a MCPWM driver:

LPC175x_6x CMSIS-Compliant Standard Peripheral Firmware Driver Library (Keil, IAR, GNU) | www.LPCwar... 

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply