DSP capabilities on LPC54102

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSP capabilities on LPC54102

3,029 Views
skanda19
Contributor III

Hello, 

does the LPC54102 have any DSP capabilities associated with the ADC or peripheral ? 

Labels (1)
Tags (3)
0 Kudos
Reply
4 Replies

3,000 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @skanda19 

Sorry there isn't. There is ADC demo under SDK, can download from:

https://mcuxpresso.nxp.com/en/select  

 

BR

Alice

0 Kudos
Reply

2,979 Views
skanda19
Contributor III

thanks for your reply @Alice_Yang.

Another questions comes to mind, I know that the LPC54102 max sampling rate for the ADC is 5Mhz. But I assume this is only using one channel, how does the BW of the sampling rate of the ADC behaves if I add more channels ??? is the sampling rate get divided by the # of channels or it has the same 5 MHz for each channel ?  

 

 

thanks!

0 Kudos
Reply

2,937 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @skanda19 

"is the sampling rate get divided by the # of channels "

->> YES,

 

Alice

 

0 Kudos
Reply

2,897 Views
skanda19
Contributor III
Thanks Alice!!!
0 Kudos
Reply