DSP Sample code for LPC4367

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSP Sample code for LPC4367

2,152 Views
gauravmore
Contributor III

I am new to CMSIS library in LPC Expresso. Is ther any reference code which provides the functionality and understanding of DSP library in order to check the FFT output  by sending the samples recieved?

Please provide the solution or reference code for the same, since cannot find it in the code bundle provided in LPCexpresso.

Labels (2)
0 Kudos
Reply
2 Replies

1,851 Views
converse
Senior Contributor V

This may be helpful to you:

CMSIS DSP Library Support 

The library can be found in the Examples directory of the MCUXpresso install.

0 Kudos
Reply

1,851 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Gaurav More,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to LPC43xx CMSIS-Compliant Standard Peripheral Firmware Driver Library whose link is below.

Have a great day.
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 Kudos
Reply