DMA Request Select register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA Request Select register

1,112件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by John Sinclair on Thu Jul 26 02:33:44 MST 2012
Hello,

did I understand right:
With the LPC1778 I can't use a DMA with peripheral UART0 (transmit) and UART3 (transmit) at the same time?
Thanks for answer
ラベル(1)
0 件の賞賛
返信
1 返信

1,096件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by John Sinclair on Thu Jul 26 06:46:14 MST 2012
incredible but true! A lot of combinations of DMA requests are not possible because always two requests share one bit!
Why? I don't know, in this register are 16 bits reserved!
Very bad design! The DMA loss a lot of his power!
0 件の賞賛
返信