DFUSec: command line

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DFUSec: command line

1,721 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fcarlo on Thu Jun 27 10:55:34 MST 2013

Hi all,


I would like to know if there is any plan to release a a command line version of the DFUSec tool.


Regards 

标签 (1)
0 项奖励
回复
3 回复数

1,690 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lancos_com on Tue Nov 19 01:34:14 MST 2013
Hi,
I implemented a command line interface for DFU + bash script to program and verify SPIFI flash on LPC1850, if you are interested you can download the file here http://www.lancos.com/lpc_dfu-1.02.tar.gz
Claudio
0 项奖励
回复

1,690 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fcarlo on Thu Jun 27 23:43:44 MST 2013

Thank you for your kind answer.
We would like to have a much simpler interface (or a script) to give it to our production facility.

0 项奖励
回复

1,690 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Thu Jun 27 12:03:00 MST 2013

We've tossed this idea around in the past and it was always a 'maybe', but never quite important enough to actually implement.


It might be easily possible to add a switch to allow loading alternate configuration files (so you can perform different auto-program sequences based on the configuraiton file you select, but adding individual command-line options for the many configuration options in the DFU Utility might take some time.


What do you need a command line verison of the tool to do?

0 项奖励
回复