DFU programmer through USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DFU programmer through USB

8,374 Views
andrewbarningha
Contributor III

Is it possible anyone can give me some advice on downloading firmware through a USB port to the MCB1800 dev board.

 

My program builds OK and can run when I download firmware through the serial port or when using JTAG, but when I use the DFU programmer through the USB port it downloads OK but my program won't run.

Is there anything anyone can suggest from the screen shots attached.

Thanks

Andrew

3 Replies

7,967 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Andrew,

Have you considered using LPCScrypt instead?


http://www.lpcware.com/lpcscrypt

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

7,967 Views
andrewbarningha
Contributor III

Hi Carlos,

Thanks for that.

I have also tried the LPCScrypt but had no luck.

Using LPCScrypt I can blank check and erase banka OK, i can download the binary file OK but my program won't run.

I know my code is OK because if i use JTAG or download the firmware through the serial port the code runs fine.

When i compare the binary file created with the data from address 0x1a000000 when in debug, they compare the same.

I guess my binary file is wrong but i have used keil in the past to generate binary files and it works OK, i just seem to have a problem with the LPC1857.

Any other suggestions would be appreciated.

Thanks

Andrew

0 Kudos
Reply

7,967 Views
converse
Senior Contributor V

Looks like you have not set the image checksum .

https://community.nxp.com/thread/389046