DFU Firmware Update Utility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DFU Firmware Update Utility

1,978件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gregd on Thu Jan 19 09:52:39 MST 2012
Does anyone know where to get the DFU Firmware Update Utility that would be compatible with the LPC4350?
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,856件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpc18_43 on Wed Apr 04 13:45:12 MST 2012
This issue has been solved.  USB DFU Download and Upload using DFU-Util works fine on the LPC18xx and LPC43xx:

http://knowledgebase.nxp.com/showthread.php?p=15454#post15454
0 件の賞賛
返信

1,856件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpc18_43 on Mon Mar 26 18:25:06 MST 2012
Any updates?  Have you managed to get it to work?

I have attempted to use dfu-util to download firmware onto the LPC1850 but it fails.  The '-' revision ROM DFU code appears to incorrectly respond to a DFU_GETSTATUS request.  Does DFU boot work on 'A' revision parts?

I have posted technical details on the NXP Knowledgebase (need to log in to see image):
http://www.lpcware.com/showthread.php?t=3042

Any advice will be appreciated.
0 件の賞賛
返信

1,856件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by trioflex on Mon Jan 23 03:20:35 MST 2012
We have not found any :(

It enumerates as

VID: 1FC9
PID: 000C

installed libusb, and trying dfu-util

it can download from LPC4350 something, but well uploading junk freezes.. I do not have any image yet to upload. So maybe maybe it would work if feeding proper boot image

Antti
0 件の賞賛
返信