DELETE FIRMWARE LPC1227

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DELETE FIRMWARE LPC1227

1,508件の閲覧回数
3L1S4_
Contributor I

Hi,
I bought some components code LPC1227FBD48/301EL but I can't use them.

I think they have already been used so a firmware is already present.

Can someone help me delete it?

What program can I use to restore the component and rewrite a new firmware?

Thanks all in advance

0 件の賞賛
返信
3 返答(返信)

1,475件の閲覧回数
3L1S4_
Contributor I

Hi Pavel,

thanks for your quick reply.

We generally use this software (to write firmware) FLASH MAGIC.

Do you know it? Is the procedure to erase all memory the same?

Thanks so much,

Best Regard

0 件の賞賛
返信

1,459件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I do not use the flash magic before, but I download it, could you try to select on the erase section entire device?

Pavel_Hernandez_0-1725470684812.png

And then start. Let me know if this help you.

Best regards,
Pavel

0 件の賞賛
返信

1,486件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, there are two ways to do a mass erase, you could use the IDE with your debugger probe.

Look at the image use it at example, just need to know what kind of debugger you have.

Pavel_Hernandez_0-1725400979838.png

The other way if you do not have the debugger maybe you could use the Uart and use the ISP mode on the MCU, then use the BLHOST to send a come for erase all memory.

Best regards,
Pavel

 

0 件の賞賛
返信