DALI mcu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DALI mcu

1,814 Views
邱海耀
Contributor I

hi I want to manufacturer a DALI, LED power, so I can use LPC1114 directly? without more software? in other word, we only need to put this IC into PCB, then it is fine? please feedback me..

Labels (1)
0 Kudos
Reply
1 Reply

1,563 Views
soledad
NXP Employee
NXP Employee

Hi,

The device does not have pre-loaded the program, therefore it is necessary to program the device with the desired software.

Please check the AN11174, this application note describes how to create a DALI slave device with the OM13026 LPC111x DALI slave board.

http://www.mouser.be/pdfdocs/AN11174.pdf 

DALI on LPC Microcontrollers 

Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply