DALI Development Kit Revision 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DALI Development Kit Revision 2

2,180 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by oyvindsc on Fri Jun 20 05:31:52 MST 2014
Hi,

The DALI 2.0 SDK contains a static library that does all the DALI magic, the source code is not included.

Is it possible to release the source for this library? I need to extend the implementation for a demo, and it would be a real time saver to have the source code.

Thanks and Regards,
Øyvind
Labels (1)
0 Kudos
Reply
2 Replies

1,936 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp_apps on Fri Jun 20 12:35:44 MST 2014
Hi,

We do not provide the source code for the library.
If your annual volume is very high, please try contacting an NXP FAE in your region.

Thanks.

nxp support
0 Kudos
Reply

1,936 Views
gintarasdruktei
Contributor II

Hi,

If NXP cannot provide the source code for DALI library, at least could you confirm that it is fully compatible with LPC1115?

I have started new project with LPC1115 and it seems that this library does not initialize CT16B0 timer correctly. I cannot find any bugs in my program and I cannot check what's in that library, it is very frustrating...

Regards,

Gintaras

0 Kudos
Reply