DAC to LPC54616

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DAC to LPC54616

1,067 Views
Nadia
Contributor III

Good morning,


I was wondering if someone could recommend a DAC for use with the LPC54616 microcontroller, which is powered at 3.3V.


The aim is to convert a PWM signal generated by the microcontroller into a triangular signal.


Best regards.

0 Kudos
Reply
1 Reply

1,048 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

NXP has 8-bit I2C A/D and D/A converter PCF8591. Operating supply voltage 2.5 V to 6.0 V

https://www.nxp.com/products/interfaces/ic-spi-serial-interface-devices/ic-dacs-and-adcs/8-bit-a-d-a...

For more DAC, I suggest you checking 3rd parties, for example ADI.

 

Have a nice day,

Jun Zhang

0 Kudos
Reply