DAC VREF dependency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DAC VREF dependency

1,427 Views
TRCooper
Contributor II

Using LPC553x for a low power application.  Reference Manual Rev 3, 07/2023. Paragraph 48.1.4 DAC Chip-specific Initialization states: "Enable VREF module...  DAC PTAT and ZTC current sources come from VREF module."   What is the lowest power configuration of VREF that is needed for use of the DACs?  Does VREF buffering need to be enabled?  Using external reference for DAC reference select but DAC still apparently requires VREF for current source. Is there guidance regarding selection of PTAT vs ZTC, and what the tradeoffs are?  Thanks.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,382 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

For minimum power, you can configure VREF in bandgap-only mode and disable unnecessary features. Buffering is not required if you are not using VREF_OUT as the DAC reference.
More details for VREF, please refer to the attached presentations on this post: LPC5536: on DAC current sources (ZTC, PTAT)

BR,
Omar

0 Kudos
Reply