DAC / ADC sharing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DAC / ADC sharing

跳至解决方案
2,072 次查看
tonyvink
Contributor II

Not sure if I am reading the users manual correctly for the LPC1837...

Concerning sharing DAC and ADC0, if I am using the DAC on pin B2, is the ADC0_0 unavailable on package position C2.  I am using the LBGA256 package.  

Thanks

1 解答
1,932 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tony,

You are correct, the use of the DAC blocks channel 0 of both ADC0 and ADC1. The reason is that the ADC0_0/ADC1_0/DAC pin hardwires them all together.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

在原帖中查看解决方案

2 回复数
1,931 次查看
tonyvink
Contributor II

Thanks Carlos.

I would have replied sooner but I guess I was looking in the wrong place.  Thought I posted in the LPC1837 section but guess I messed something up when posting.

1,933 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tony,

You are correct, the use of the DAC blocks channel 0 of both ADC0 and ADC1. The reason is that the ADC0_0/ADC1_0/DAC pin hardwires them all together.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer