Custom bootloader memory config issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Custom bootloader memory config issue

4,474 Views
BerkantCiftci2001
Contributor II

Hi all,

I am a student Embedded systems and I am trying to make a small custom bootloader work on my LPC1758. What I am trying to do is flash my bootloader between 0x0000 and 0x8000. My next step (for testing purposes) is to flash my application after 0x8000. However, when I let the program run, It will crash when it jumps to the application address. (see image below.)

address.jpg

I had the feeling that I had to change my project memory settings. After some research and trials, I could't work it out. (first one is bootloader, second one is application)

memory config bootloader.jpg

Memory config application.jpg

 

 

 

 

 

 

 

 

Does anyone have an idea how I should set this up correctly?

Kind regards.

 

Update: This is what I get back.

error.jpg

Labels (2)
0 Kudos
Reply
5 Replies

4,427 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @BerkantCiftci2001 

1) First please confirm the application can work well without bootloader.

2)Confirm bootloader program application image correctly.

3) Confirm bootloader can jump to application.

4) There is USB secondary bootloader for lpc1700, you can refer to the jump code :

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...  

5) And there is debug application with MCUXpresso IDE method:

 https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/8... 

 

BR

Alice

 

 

 

0 Kudos
Reply

4,415 Views
BerkantCiftci2001
Contributor II

Hi @Alice_Yang , Thanks for your reply! I would like to know more about the memory mapping. Should the application have a seperate size too? What I am trying is the following:

  1. flash bootloader.
  2. flash my application second with second MCUXpresso instance.
  3. let the bootloader code run through the jumping process. 

This works good. But when I try to flash my application with my custom software, the bootloader gives me UNDEFINED INSTRUCTION. I checked the .hex file and this is written correctly into the memory.

0 Kudos
Reply

4,395 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @BerkantCiftci2001 

 

The flash size of application should 0x80000 - 0x8000, because the total size of flash is 0x80000 (512k),

bootloader uses 0x8000.

 

BR

Alice

0 Kudos
Reply

4,390 Views
BerkantCiftci2001
Contributor II

Hi @Alice_Yang ,

 

I have seperated the Flash size for bootloader and application.

Should this also be done for the RAM?

So:

  • bootloader start 0x10000000, size 0x2000
  • application start 0x10002000 size 0x6000

I still get this error at jump while debugging bootloader :

image.png

0 Kudos
Reply

4,372 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @BerkantCiftci2001 

1) From your screenshot, it application size still 0x80000:

Alice_Yang_0-1670223699441.png

 

2) RAM needn't.

 

BR

Alice

0 Kudos
Reply