Custom USB HID LPC1549 Xpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Custom USB HID LPC1549 Xpresso

1,234 Views
manmohanvishwa1
Contributor I

I want to send data every 10ms to PC using Custom USB HID mode of LPC1549.

I am using LPC1549 Xpresso Board with IAR Workbench, I tried its sample bundle of code lpcopen_2_20_keil_iar_nxp_lpcxpresso_1549 but it send data only once.

0 Kudos
Reply
1 Reply

1,167 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Manmohan Vishwakarma,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

I was wondering if you can introduce which demo selected as the template demo and modifying work you do, then I can replicate the phenomenon on my site.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply