Currently using LPC82x, but need to also use Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Currently using LPC82x, but need to also use Linux

1,211 Views
jeremyprice
Contributor I

Apologies, as I am not technical.

We have some code running on the LPC82X. However we now need to run a Linux processor. Is there a product we can use where we can port the existing code onto the upgraded processor.

Any help greatly appreciated.

Jeremy

0 Kudos
Reply
1 Reply

1,150 Views
soledad
NXP Employee
NXP Employee

Hi,

Please continue the follow up in this thread: Advice on upgrade from LPC82x to Linux based processor 


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply