Current version of files used by AN10916

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Current version of files used by AN10916

1,331 次查看
perdrix
Contributor II

The FatFs project directory contains a number of files:

 Directory of C:\Users\amonra\Downloads\NXP\LPC1700_FatFs_Prj\LPC1700\RTC

15/12/2010  14:30    <DIR>          .
15/12/2010  14:31    <DIR>          ..
09/12/2010  10:50             2,686 lpc17xx_rtc.c
09/12/2010  10:46             1,979 lpc17xx_rtc.h
               2 File(s)          4,665 bytes

 Directory of C:\Users\amonra\Downloads\NXP\LPC1700_FatFs_Prj\LPC1700\SPI_SD

15/12/2010  14:31    <DIR>          .
15/12/2010  14:31    <DIR>          ..
15/12/2010  14:24             6,355 lpc17xx_spi.c
10/12/2010  15:49             1,483 lpc17xx_spi.h
10/12/2010  16:21            21,890 sd.c
10/12/2010  14:56             2,299 sd.h
               4 File(s)         32,027 bytes

 Directory of C:\Users\amonra\Downloads\NXP\LPC1700_FatFs_Prj\LPC1700\UART

15/12/2010  14:19    <DIR>          .
15/12/2010  14:31    <DIR>          ..
15/12/2010  14:22             3,876 lpc17xx_uart.c
10/12/2010  11:37             1,463 lpc17xx_uart.h
               2 File(s)          5,339 bytes

Where can I find the up to date version of those files?  My uVision installation doesn't appear to contain any files with those names.

 

0 项奖励
回复
3 回复数

1,320 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @perdrix 

After download AN10916, we can find these files under LPC1700_FatFs_Prj project:

Alice_Yang_0-1690857517914.png

 

BR

Alice

 

0 项奖励
回复

1,312 次查看
perdrix
Contributor II

No I cannot - those are out of date versions and don't match up with the CURRENT FatFS code

I want the latest NXP versions of those files.

0 项奖励
回复

1,277 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @perdrix 

There is no update for " CURRENT FatFS code", only the files under AN10916 folder for that version FatFS.

 

BR

Alice

0 项奖励
回复