Creating my own board for LPC4337

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Creating my own board for LPC4337

1,222 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by acelink1 on Sun Mar 16 22:57:16 MST 2014
HI Guys, I've ordered a few LPC4337 LQFP 144pin MCU's and I'm going to create my own breakout board.

The only thing I'm not too sure of is the JTAG programming port.
Can someone direct me to a circuit which has the LPC4337 with a JTAG programming port.

I've researched and come up with this.  Let me know if this is wrong.

JTAG 10PIN programming port to LPC4337 LQFP144pin.

JTAG PIN 1 - +3V3
JTAG PIN 2 - JTAG_TMS with 10k pullup.
JTAG PIN 3 - GND
JTAG PIN 4 - JTAG_TCK with 10k pulldown.
JTAG PIN 5 - GND
JTAG PIN 6 - JTAG_TDO with 10k pulldown.
JTAG PIN 7 - JTAG_RTCK
JTAG PIN 8 - JTAG_TDI with 10k pullup.
JTAG PIN 9 - GND
JTAG PIN10- RESET_IN

Thanks guys and thank you for your recent support. Migrating from Atmel 32Bit to LPC is quite a challenge, but I'm getting there :)

Pete :)

Labels (1)
0 Kudos
Reply
2 Replies

1,194 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Mon Mar 17 09:12:01 MST 2014

Quote: acelink1

HI Guys, I've ordered a few LPC4337 LQFP 144pin MCU's and I'm going to create my own breakout board.



Hey Pete,
are you going to make it available to others or even sell one or two PCBs (unpopulated) ?

Will you design it in a way, that allows use of the UART ISP option? This requires generating the uC's /RESET with a common-anode diode array, to implement a logic AND. And please omit the MAX3232, stick to the 3.3V levels ;-)

0 Kudos
Reply

1,194 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Sun Mar 16 23:40:11 MST 2014
http://www.lpcware.com/content/faq/lpcxpresso/debug-design
0 Kudos
Reply