Creating Custom Board File (.mex) for MCUXPresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating Custom Board File (.mex) for MCUXPresso IDE

ソリューションへジャンプ
10,652件の閲覧回数
SrinathVelavan
Contributor III

Hi, 

I am creating a custom board using LPC55S69 as host MCU. For the purpose of adding the custom board to be used with the SDK in MCU Xpresso IDE, I am creating a custom board .mex file. 

I have configured the pin map as per my design and now working on the Clocks configuration for the board. Is there any reference for developing a custom board file using LPC55S69 Host MCU? 

I am facing difficulties configuring the clocks for the .mex file . 

TIA

 

0 件の賞賛
返信
1 解決策
10,638件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @SrinathVelavan 

What is your issue? Open clock configuration as below:

Alice_Yang_1-1687338871274.pngAlice_Yang_1-1687338871274.png

Then config in left and right parts as below:

Alice_Yang_2-1687338948746.pngAlice_Yang_2-1687338948746.png

And there is a user guide for config tools, attach it for you.

 

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
10,639件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @SrinathVelavan 

What is your issue? Open clock configuration as below:

Alice_Yang_1-1687338871274.pngAlice_Yang_1-1687338871274.png

Then config in left and right parts as below:

Alice_Yang_2-1687338948746.pngAlice_Yang_2-1687338948746.png

And there is a user guide for config tools, attach it for you.

 

 

BR

Alice

0 件の賞賛
返信
10,632件の閲覧回数
SrinathVelavan
Contributor III

Thanks for the Userguide. I have actually customized the pins as per my design. I am right now doing the clocks but there is no change in the clock sources in my design, I am using the default clock source configuration as per the LPC55S69EVK. 

Is the max clock frequency 150MHz for the LPC55S69? Just want to makesure what I have done is right. ( Refer image attached).

 

0 件の賞賛
返信