Could you help to provide OTP_READ demo code for LPC54608

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could you help to provide OTP_READ demo code for LPC54608

1,317 Views
angusshi
Contributor I

Could you help to provide OTP_READ demo code for LPC54608?

Labels (1)
0 Kudos
Reply
1 Reply

1,282 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Angus Shi,

There is an OTP demo under  SDK, pastedImage_1.png

you can combine  with OTP APIs in " UM-> Chapter 46: LPC546xx One-Time Programmable (OTP)
memory and API " .

If still have question , please contact us.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply