Could the LPC551x ISP via High-Speed crystal support @24Mhz?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Could the LPC551x ISP via High-Speed crystal support @24Mhz?

852 次查看
StephenYeh
Contributor III

Hi Sir,

I check the datasheet of LPC551x, the external crystal supports up to 25Mhz
, the customer wants to use the USB High-Speed ISP function, the spec. only 16MHz.
Could the LPC551x ISP via High-Speed crystal support @24Mhz(external crystal)?

0 项奖励
回复
1 回复

839 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi StephenYeh 

Table 194 of UM11295 has a remark that states: “For USB HS ISP mode, 16 MHz crystal is required, and for the USB FS ISP mode, ROM uses FRO”. That's to say, we can't use 24M crystal for USB HS.

ZhangJennie_1-1673443841042.png

Have a nice day,

Jun Zhang

 

0 项奖励
回复