Could NXP provide the LPC1549JDB100 reference design schematic diagram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could NXP provide the LPC1549JDB100 reference design schematic diagram

1,256件の閲覧回数
haopengtang
Contributor I

I use LPC1549JDB100 in my project . But the min system can not work! So I need the LPC1549JDB100 reference design schematic diagram.

ラベル(1)
0 件の賞賛
返信
1 返信

1,134件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

The Figure below shows the basic board connections used to power the LPC15xx, connect the external crystal and the 32kHz oscillator for the RTC, and provide debug capabilities via the serial wire port.

pastedImage_1.png

In addition you can use the OM13056 LPCXpresso board for LPC1549 as reference.

http://www.nxp.com/assets/downloads/data/en/schematics/LPC1549_LPCXpresso_v2_schem_Rev_C.pdf 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信