Cortex-M7 (IMXRT1171) crash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cortex-M7 (IMXRT1171) crash

1,742 次查看
Nexus76
Contributor II
 

TIMXRT1171.gif

0 项奖励
回复
5 回复数

1,712 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Could you please more details of this? Only when you add the root clock of CM4 the issue no longer happens?
This is strange since even when enabling M4 root, the M7 does not executes this part of the code as it is not compiled on M7 core.

#if __CORTEX_M == 4
    rootCfg.mux = kCLOCK_M4_ClockRoot_MuxOscRc48MDiv2;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_M4, &rootCfg);
#endif

I think that the cause of this is the enablement of a PLL steps before core clock. Could you please detail the exact clock that enabled solves the issue?

Best regards,
Omar

0 项奖励
回复

1,696 次查看
Nexus76
Contributor II

Thanks Omar,

I have inserted the code generated form MCUXpresso with ConfigTool->Clocks (that we use in our application)

 

 

/*
 * How to setup clock using clock driver functions:
 *
 * 1. Call CLOCK_InitXXXPLL() to configure corresponding PLL clock.
 *
 * 2. Call CLOCK_InitXXXpfd() to configure corresponding PLL pfd clock.
 *
 * 3. Call CLOCK_SetRootClock() to configure corresponding module clock source and divider.
 *
 */

/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!GlobalInfo
product: Clocks v11.0
processor: MIMXRT1171xxxxx
package_id: MIMXRT1171CVM8A
mcu_data: ksdk2_0
processor_version: 13.0.2
 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/

#include "clock_config.h"
#include "fsl_iomuxc.h"
#include "fsl_dcdc.h"
#include "fsl_pmu.h"
#include "fsl_clock.h"

/*******************************************************************************
 * Definitions
 ******************************************************************************/

/*******************************************************************************
 * Variables
 ******************************************************************************/

/*******************************************************************************
 ************************ BOARD_InitBootClocks function ************************
 ******************************************************************************/
void BOARD_InitBootClocks(void)
{
    BOARD_BootClockRUN();
}

#if defined(XIP_BOOT_HEADER_ENABLE) && (XIP_BOOT_HEADER_ENABLE == 1)
#if defined(XIP_BOOT_HEADER_DCD_ENABLE) && (XIP_BOOT_HEADER_DCD_ENABLE == 1)
/* This function should not run from SDRAM since it will change SEMC configuration. */
AT_QUICKACCESS_SECTION_CODE(void UpdateSemcClock(void));
void UpdateSemcClock(void)
{
    /* Enable self-refresh mode and update semc clock root to 200MHz. */
    SEMC->IPCMD = 0xA55A000D;
    while ((SEMC->INTR & 0x3) == 0)
        ;
    SEMC->INTR                                = 0x3;
    SEMC->DCCR                                = 0x0B;
    /*
    * Currently we are using SEMC parameter which fit both 166MHz and 200MHz, only
    * need to change the SEMC clock root here. If customer is using their own DCD and
    * want to switch from 166MHz to 200MHz, extra SEMC configuration might need to be
    * adjusted here to fine tune the SDRAM performance
    */
    CCM->CLOCK_ROOT[kCLOCK_Root_Semc].CONTROL = 0x602;
}
#endif
#endif

/*******************************************************************************
 ********************** Configuration BOARD_BootClockRUN ***********************
 ******************************************************************************/
/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!Configuration
name: BOARD_BootClockRUN
called_from_default_init: true
outputs:
- {id: ACMP_CLK_ROOT.outFreq, value: 24 MHz}
- {id: ADC1_CLK_ROOT.outFreq, value: 24 MHz}
- {id: ADC2_CLK_ROOT.outFreq, value: 24 MHz}
- {id: ARM_PLL_CLK.outFreq, value: 1.56 GHz}
- {id: ASRC_CLK_ROOT.outFreq, value: 24 MHz}
- {id: AXI_CLK_ROOT.outFreq, value: 780 MHz}
- {id: BUS_CLK_ROOT.outFreq, value: 240 MHz}
- {id: BUS_LPSR_CLK_ROOT.outFreq, value: 160 MHz}
- {id: CCM_CLKO1_CLK_ROOT.outFreq, value: 24 MHz}
- {id: CCM_CLKO2_CLK_ROOT.outFreq, value: 24 MHz}
- {id: CSSYS_CLK_ROOT.outFreq, value: 132 MHz}
- {id: CSTRACE_CLK_ROOT.outFreq, value: 24 MHz}
- {id: ENET1_CLK_ROOT.outFreq, value: 24 MHz}
- {id: ENET2_CLK_ROOT.outFreq, value: 125 MHz}
- {id: ENET_1G_TX_CLK.outFreq, value: 125 MHz}
- {id: ENET_25M_CLK_ROOT.outFreq, value: 24 MHz}
- {id: ENET_QOS_CLK_ROOT.outFreq, value: 24 MHz}
- {id: ENET_TIMER1_CLK_ROOT.outFreq, value: 24 MHz}
- {id: ENET_TIMER2_CLK_ROOT.outFreq, value: 24 MHz}
- {id: ENET_TIMER3_CLK_ROOT.outFreq, value: 24 MHz}
- {id: FLEXIO1_CLK_ROOT.outFreq, value: 24 MHz}
- {id: FLEXIO2_CLK_ROOT.outFreq, value: 24 MHz}
- {id: FLEXSPI1_CLK_ROOT.outFreq, value: 24 MHz}
- {id: FLEXSPI2_CLK_ROOT.outFreq, value: 198 MHz}
- {id: GPT1_CLK_ROOT.outFreq, value: 24 MHz}
- {id: GPT1_ipg_clk_highfreq.outFreq, value: 24 MHz}
- {id: GPT2_CLK_ROOT.outFreq, value: 24 MHz}
- {id: GPT2_ipg_clk_highfreq.outFreq, value: 24 MHz}
- {id: GPT3_CLK_ROOT.outFreq, value: 24 MHz}
- {id: GPT3_ipg_clk_highfreq.outFreq, value: 24 MHz}
- {id: GPT4_CLK_ROOT.outFreq, value: 24 MHz}
- {id: GPT4_ipg_clk_highfreq.outFreq, value: 24 MHz}
- {id: GPT5_CLK_ROOT.outFreq, value: 24 MHz}
- {id: GPT5_ipg_clk_highfreq.outFreq, value: 24 MHz}
- {id: GPT6_CLK_ROOT.outFreq, value: 200/3 MHz}
- {id: GPT6_ipg_clk_highfreq.outFreq, value: 200/3 MHz}
- {id: LPI2C1_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPI2C2_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPI2C3_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPI2C4_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPI2C5_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPI2C6_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPSPI1_CLK_ROOT.outFreq, value: 172.8/7 MHz}
- {id: LPSPI2_CLK_ROOT.outFreq, value: 172.8/7 MHz}
- {id: LPSPI3_CLK_ROOT.outFreq, value: 172.8/7 MHz}
- {id: LPSPI4_CLK_ROOT.outFreq, value: 172.8/7 MHz}
- {id: LPSPI5_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPSPI6_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART10_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART11_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART12_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART1_CLK_ROOT.outFreq, value: 200/3 MHz}
- {id: LPUART2_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART3_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART4_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART5_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART6_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART7_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART8_CLK_ROOT.outFreq, value: 24 MHz}
- {id: LPUART9_CLK_ROOT.outFreq, value: 24 MHz}
- {id: M7_CLK_ROOT.outFreq, value: 780 MHz}
- {id: M7_SYSTICK_CLK_ROOT.outFreq, value: 50 MHz}
- {id: OSC_24M.outFreq, value: 24 MHz}
- {id: OSC_32K.outFreq, value: 32.768 kHz}
- {id: OSC_RC_16M.outFreq, value: 16 MHz}
- {id: OSC_RC_400M.outFreq, value: 400 MHz}
- {id: OSC_RC_48M.outFreq, value: 48 MHz}
- {id: OSC_RC_48M_DIV2.outFreq, value: 24 MHz}
- {id: SYS_PLL1_CLK.outFreq, value: 1 GHz, locked: true, accuracy: '0.001'}
- {id: SYS_PLL1_DIV2_CLK.outFreq, value: 500 MHz}
- {id: SYS_PLL2_CLK.outFreq, value: 528 MHz}
- {id: SYS_PLL2_PFD1_CLK.outFreq, value: 9504/19 MHz}
- {id: SYS_PLL2_PFD2_CLK.outFreq, value: 594 MHz}
- {id: SYS_PLL2_PFD3_CLK.outFreq, value: 1900.8/7 MHz}
- {id: SYS_PLL2_SS_MODULATION.outFreq, value: 1.2 kHz}
- {id: SYS_PLL2_SS_RANGE.outFreq, value: 12 MHz}
- {id: SYS_PLL3_CLK.outFreq, value: 480 MHz}
- {id: SYS_PLL3_DIV2_CLK.outFreq, value: 240 MHz}
- {id: USDHC1_CLK_ROOT.outFreq, value: 24 MHz}
- {id: USDHC2_CLK_ROOT.outFreq, value: 24 MHz}
settings:
- {id: SOCDomainVoltage, value: OD}
- {id: ANADIG_OSC_OSC_24M_CTRL_LP_EN_CFG, value: Low}
- {id: ANADIG_OSC_OSC_24M_CTRL_OSC_EN_CFG, value: Enabled}
- {id: ANADIG_PLL.ARM_PLL_POST_DIV.scale, value: '1', locked: true}
- {id: ANADIG_PLL.ARM_PLL_PREDIV.scale, value: '1', locked: true}
- {id: ANADIG_PLL.ARM_PLL_VDIV.scale, value: '65', locked: true}
- {id: ANADIG_PLL.PLL_AUDIO_BYPASS.sel, value: ANADIG_OSC.OSC_24M}
- {id: ANADIG_PLL.PLL_VIDEO_BYPASS.sel, value: ANADIG_OSC.OSC_24M}
- {id: ANADIG_PLL.SYS_PLL2.denom, value: '20000', locked: true}
- {id: ANADIG_PLL.SYS_PLL2.div, value: '22'}
- {id: ANADIG_PLL.SYS_PLL2.num, value: '0', locked: true}
- {id: ANADIG_PLL.SYS_PLL2_PFD1_DIV.scale, value: '19', locked: true}
- {id: ANADIG_PLL.SYS_PLL2_PFD1_MUL.scale, value: '18', locked: true}
- {id: ANADIG_PLL.SYS_PLL2_PFD2_DIV.scale, value: '16', locked: true}
- {id: ANADIG_PLL.SYS_PLL2_PFD2_MUL.scale, value: '18', locked: true}
- {id: ANADIG_PLL.SYS_PLL2_PFD3_DIV.scale, value: '35', locked: true}
- {id: ANADIG_PLL.SYS_PLL2_PFD3_MUL.scale, value: '18', locked: true}
- {id: ANADIG_PLL.SYS_PLL2_SS_DIV.scale, value: '20000'}
- {id: ANADIG_PLL.SYS_PLL2_SS_MOD_DIV.scale, value: '20000'}
- {id: ANADIG_PLL.SYS_PLL2_SS_STEP.scale, value: '1', locked: true}
- {id: ANADIG_PLL.SYS_PLL2_SS_STOP.scale, value: '10000', locked: true}
- {id: ANADIG_PLL.SYS_PLL3_PFD3_DIV.scale, value: '13', locked: true}
- {id: ANADIG_PLL.SYS_PLL3_PFD3_MUL.scale, value: '18', locked: true}
- {id: ANADIG_PLL_ARM_PLL_CTRL_POWERUP_CFG, value: Enabled}
- {id: ANADIG_PLL_PLL_AUDIO_CTRL_GATE_CFG, value: Disabled}
- {id: ANADIG_PLL_PLL_VIDEO_CTRL_GATE_CFG, value: Disabled}
- {id: ANADIG_PLL_SYS_PLL1_CTRL_SYS_PLL1_DIV2_CFG, value: Enabled}
- {id: ANADIG_PLL_SYS_PLL2_CTRL_POWERUP_CFG, value: Enabled}
- {id: ANADIG_PLL_SYS_PLL2_PFD_PFD0_DIV1_CLKGATE_CFG, value: Disabled}
- {id: ANADIG_PLL_SYS_PLL2_SS_ENABLE_CFG, value: Enabled}
- {id: ANADIG_PLL_SYS_PLL3_CTRL_POWERUP_CFG, value: Enabled}
- {id: ANADIG_PLL_SYS_PLL3_CTRL_SYS_PLL3_DIV2_CFG, value: Enabled}
- {id: ANADIG_PLL_SYS_PLL3_PFD_PFD0_DIV1_CLKGATE_CFG, value: Disabled}
- {id: ANADIG_PLL_SYS_PLL3_PFD_PFD1_DIV1_CLKGATE_CFG, value: Disabled}
- {id: ANADIG_PLL_SYS_PLL3_PFD_PFD2_DIV1_CLKGATE_CFG, value: Disabled}
- {id: ANADIG_PLL_SYS_PLL3_PFD_PFD3_DIV1_CLKGATE_CFG, value: Disabled}
- {id: CCM.CLOCK_ROOT0.DIV.scale, value: '2', locked: true}
- {id: CCM.CLOCK_ROOT0.MUX.sel, value: ANADIG_PLL.ARM_PLL_CLK}
- {id: CCM.CLOCK_ROOT1.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT10.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT11.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT12.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT13.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT14.DIV.scale, value: '1', locked: true}
- {id: CCM.CLOCK_ROOT14.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT15.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT16.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT17.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT18.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT19.DIV.scale, value: '6', locked: true}
- {id: CCM.CLOCK_ROOT19.MUX.sel, value: ANADIG_OSC.OSC_RC_400M}
- {id: CCM.CLOCK_ROOT2.DIV.scale, value: '2', locked: true}
- {id: CCM.CLOCK_ROOT2.MUX.sel, value: ANADIG_PLL.SYS_PLL3_CLK}
- {id: CCM.CLOCK_ROOT20.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT21.DIV.scale, value: '3', locked: true}
- {id: CCM.CLOCK_ROOT21.MUX.sel, value: ANADIG_PLL.SYS_PLL2_PFD2_CLK}
- {id: CCM.CLOCK_ROOT22.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT23.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT24.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT25.DIV.scale, value: '6', locked: true}
- {id: CCM.CLOCK_ROOT25.MUX.sel, value: ANADIG_OSC.OSC_RC_400M}
- {id: CCM.CLOCK_ROOT26.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT27.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT28.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT29.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT3.DIV.scale, value: '3', locked: true}
- {id: CCM.CLOCK_ROOT3.MUX.sel, value: ANADIG_PLL.SYS_PLL3_CLK}
- {id: CCM.CLOCK_ROOT30.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT31.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT32.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT33.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT34.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT35.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT36.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT37.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT38.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT39.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT4.DIV.scale, value: '3', locked: true}
- {id: CCM.CLOCK_ROOT4.MUX.sel, value: ANADIG_PLL.SYS_PLL2_PFD1_CLK}
- {id: CCM.CLOCK_ROOT40.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT41.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT42.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT43.DIV.scale, value: '11', locked: true}
- {id: CCM.CLOCK_ROOT43.MUX.sel, value: ANADIG_PLL.SYS_PLL2_PFD3_CLK}
- {id: CCM.CLOCK_ROOT44.DIV.scale, value: '11', locked: true}
- {id: CCM.CLOCK_ROOT44.MUX.sel, value: ANADIG_PLL.SYS_PLL2_PFD3_CLK}
- {id: CCM.CLOCK_ROOT45.DIV.scale, value: '11', locked: true}
- {id: CCM.CLOCK_ROOT45.MUX.sel, value: ANADIG_PLL.SYS_PLL2_PFD3_CLK}
- {id: CCM.CLOCK_ROOT46.DIV.scale, value: '11', locked: true}
- {id: CCM.CLOCK_ROOT46.MUX.sel, value: ANADIG_PLL.SYS_PLL2_PFD3_CLK}
- {id: CCM.CLOCK_ROOT47.DIV.scale, value: '1', locked: true}
- {id: CCM.CLOCK_ROOT47.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT48.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT49.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT5.DIV.scale, value: '4', locked: true}
- {id: CCM.CLOCK_ROOT5.MUX.sel, value: ANADIG_PLL.SYS_PLL2_CLK}
- {id: CCM.CLOCK_ROOT50.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT51.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT52.DIV.scale, value: '4', locked: true}
- {id: CCM.CLOCK_ROOT52.MUX.sel, value: ANADIG_PLL.SYS_PLL1_DIV2_CLK}
- {id: CCM.CLOCK_ROOT53.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT54.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT55.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT56.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT57.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT58.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT59.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT6.DIV.scale, value: '1', locked: true}
- {id: CCM.CLOCK_ROOT6.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT60.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT61.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT62.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT63.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT64.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT65.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT66.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT67.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT68.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT69.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT7.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT70.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT71.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT72.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT73.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT74.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT75.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT76.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT77.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT78.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM.CLOCK_ROOT8.DIV.scale, value: '8', locked: true}
- {id: CCM.CLOCK_ROOT8.MUX.sel, value: ANADIG_OSC.OSC_RC_400M}
- {id: CCM.CLOCK_ROOT9.MUX.sel, value: ANADIG_OSC.OSC_24M}
- {id: CCM_CLOCK_ROOT1_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT22_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT23_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT24_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT49_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT50_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT61_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT62_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT63_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT64_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT65_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT66_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT67_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT68_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT69_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT70_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT71_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT72_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT73_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT74_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT75_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT76_CONTROL_OFF_CFG, value: 'Off'}
- {id: CCM_CLOCK_ROOT7_CONTROL_OFF_CFG, value: 'Off'}
- {id: CLK_ROOT4_INIT_Config, value: disabled}
- {id: OSC_RC_400M_CTRL3_EN_1M_CLK_CFG, value: Disabled}
 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/

/*******************************************************************************
 * Variables for BOARD_BootClockRUN configuration
 ******************************************************************************/

#ifndef SKIP_POWER_ADJUSTMENT
#if __CORTEX_M == 7
#define BYPASS_LDO_LPSR 1
#define SKIP_LDO_ADJUSTMENT 1
#elif __CORTEX_M == 4
#define SKIP_DCDC_ADJUSTMENT 1
#define SKIP_FBB_ENABLE 1
#endif
#endif

const clock_arm_pll_config_t armPllConfig_BOARD_BootClockRUN =
    {
        .postDivider = kCLOCK_PllPostDiv1,        /* Post divider, 0 - DIV by 2, 1 - DIV by 4, 2 - DIV by 8, 3 - DIV by 1 */
        .loopDivider = 130,                       /* PLL Loop divider, Fout = Fin * ( loopDivider / ( 2 * postDivider ) ) */
    };

const clock_sys_pll1_config_t sysPll1Config_BOARD_BootClockRUN =
    {
        .pllDiv2En = 1,                           /* Enable Sys Pll1 divide-by-2 clock or not */
        .pllDiv5En = 0,                           /* Enable Sys Pll1 divide-by-5 clock or not */
        .ss = NULL,                               /* Spread spectrum parameter */
        .ssEnable = false,                        /* Enable spread spectrum or not */
    };

clock_pll_ss_config_t sysPll2SsConfig_BOARD_BootClockRUN =
    {
        .stop = 10000,                            /* Stop value to get frequency change */
        .step = 1,                                /* Step value to get frequency change */
    };

const clock_sys_pll2_config_t sysPll2Config_BOARD_BootClockRUN =
    {
        .mfd = 20000,                             /* Denominator of spread spectrum */
        .ss = &sysPll2SsConfig_BOARD_BootClockRUN,/* Spread spectrum parameter */
        .ssEnable = true,                         /* Enable spread spectrum or not */
    };

/*******************************************************************************
 * Code for BOARD_BootClockRUN configuration
 ******************************************************************************/
void BOARD_BootClockRUN(void)
{
    clock_root_config_t rootCfg = {0};

    /* Set DCDC to DCM mode to improve the efficiency for light loading in run mode and transient performance with a big loading step. */
    DCDC_BootIntoDCM(DCDC);

#if !defined(SKIP_DCDC_ADJUSTMENT) || (!SKIP_DCDC_ADJUSTMENT)
    if((OCOTP->FUSEN[16].FUSE == 0x57AC5969U) && ((OCOTP->FUSEN[17].FUSE & 0xFFU) == 0x0BU))
    {
        DCDC_SetVDD1P0BuckModeTargetVoltage(DCDC, kDCDC_1P0BuckTarget1P15V);
    }
    else
    {
        /* Set 1.125V for production samples to align with data sheet requirement */
        DCDC_SetVDD1P0BuckModeTargetVoltage(DCDC, kDCDC_1P0BuckTarget1P125V);
    }
#endif

#if !defined(SKIP_FBB_ENABLE) || (!SKIP_FBB_ENABLE)
    /* Check if FBB need to be enabled in OverDrive(OD) mode */
    if(((OCOTP->FUSEN[7].FUSE & 0x10U) >> 4U) != 1)
    {
        PMU_EnableBodyBias(ANADIG_PMU, kPMU_FBB_CM7, true);
    }
    else
    {
        PMU_EnableBodyBias(ANADIG_PMU, kPMU_FBB_CM7, false);
    }
#endif

#if defined(BYPASS_LDO_LPSR) && BYPASS_LDO_LPSR
    PMU_StaticEnableLpsrAnaLdoBypassMode(ANADIG_LDO_SNVS, true);
    PMU_StaticEnableLpsrDigLdoBypassMode(ANADIG_LDO_SNVS, true);
#endif

#if !defined(SKIP_LDO_ADJUSTMENT) || (!SKIP_LDO_ADJUSTMENT)
    pmu_static_lpsr_ana_ldo_config_t lpsrAnaConfig;
    pmu_static_lpsr_dig_config_t lpsrDigConfig;

    if((ANADIG_LDO_SNVS->PMU_LDO_LPSR_ANA & ANADIG_LDO_SNVS_PMU_LDO_LPSR_ANA_BYPASS_MODE_EN_MASK) == 0UL)
    {
        PMU_StaticGetLpsrAnaLdoDefaultConfig(&lpsrAnaConfig);
        PMU_StaticLpsrAnaLdoInit(ANADIG_LDO_SNVS, &lpsrAnaConfig);
    }

    if((ANADIG_LDO_SNVS->PMU_LDO_LPSR_DIG & ANADIG_LDO_SNVS_PMU_LDO_LPSR_DIG_BYPASS_MODE_MASK) == 0UL)
    {
        PMU_StaticGetLpsrDigLdoDefaultConfig(&lpsrDigConfig);
        lpsrDigConfig.targetVoltage = kPMU_LpsrDigTargetStableVoltage1P117V;
        PMU_StaticLpsrDigLdoInit(ANADIG_LDO_SNVS, &lpsrDigConfig);
    }
#endif

    /* Config CLK_1M */
    CLOCK_OSC_Set1MHzOutputBehavior(kCLOCK_1MHzOutDisable);

    /* Init OSC RC 16M */
    ANADIG_OSC->OSC_16M_CTRL |= ANADIG_OSC_OSC_16M_CTRL_EN_IRC4M16M_MASK;

    /* Init OSC RC 400M */
    CLOCK_OSC_EnableOscRc400M();
    CLOCK_OSC_GateOscRc400M(true);

    /* Init OSC RC 48M */
    CLOCK_OSC_EnableOsc48M(true);
    CLOCK_OSC_EnableOsc48MDiv2(true);

    /* Config OSC 24M */
    ANADIG_OSC->OSC_24M_CTRL |= ANADIG_OSC_OSC_24M_CTRL_OSC_EN(1) | ANADIG_OSC_OSC_24M_CTRL_BYPASS_EN(0) | ANADIG_OSC_OSC_24M_CTRL_BYPASS_CLK(0) | ANADIG_OSC_OSC_24M_CTRL_LP_EN(1) | ANADIG_OSC_OSC_24M_CTRL_OSC_24M_GATE(0);
    /* Wait for 24M OSC to be stable. */
    while (ANADIG_OSC_OSC_24M_CTRL_OSC_24M_STABLE_MASK !=
            (ANADIG_OSC->OSC_24M_CTRL & ANADIG_OSC_OSC_24M_CTRL_OSC_24M_STABLE_MASK))
    {
    }

    /* Swicth both core, M7 Systick and Bus_Lpsr to OscRC48MDiv2 first */
    rootCfg.mux = kCLOCK_M7_ClockRoot_MuxOscRc48MDiv2;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_M7, &rootCfg);

    rootCfg.mux = kCLOCK_M7_SYSTICK_ClockRoot_MuxOscRc48MDiv2;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_M7_Systick, &rootCfg);

    rootCfg.mux = kCLOCK_M4_ClockRoot_MuxOscRc48MDiv2;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_M4, &rootCfg);

    rootCfg.mux = kCLOCK_BUS_LPSR_ClockRoot_MuxOscRc48MDiv2;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Bus_Lpsr, &rootCfg);

    /*
    * if DCD is used, please make sure the clock source of SEMC is not changed in the following PLL/PFD configuration code.
    */
    /* Init Arm Pll. */
    CLOCK_InitArmPll(&armPllConfig_BOARD_BootClockRUN);

    /* Init Sys Pll1. */
    CLOCK_InitSysPll1(&sysPll1Config_BOARD_BootClockRUN);

    /* Init Sys Pll2. */
    CLOCK_InitSysPll2(&sysPll2Config_BOARD_BootClockRUN);

    /* Disable System Pll2 pfd0. */
    ANADIG_PLL->SYS_PLL2_PFD |= ANADIG_PLL_SYS_PLL2_PFD_PFD0_DIV1_CLKGATE_MASK;

    /* Init System Pll2 pfd1. */
    CLOCK_InitPfd(kCLOCK_PllSys2, kCLOCK_Pfd1, 19);

    /* Init System Pll2 pfd2. */
    CLOCK_InitPfd(kCLOCK_PllSys2, kCLOCK_Pfd2, 16);

    /* Init System Pll2 pfd3. */
    CLOCK_InitPfd(kCLOCK_PllSys2, kCLOCK_Pfd3, 35);

    /* Init Sys Pll3. */
    CLOCK_InitSysPll3();

    /* Disable System Pll3 pfd0. */
    ANADIG_PLL->SYS_PLL3_PFD |= ANADIG_PLL_SYS_PLL3_PFD_PFD0_DIV1_CLKGATE_MASK;

    /* Disable System Pll3 pfd1. */
    ANADIG_PLL->SYS_PLL3_PFD |= ANADIG_PLL_SYS_PLL3_PFD_PFD1_DIV1_CLKGATE_MASK;

    /* Disable System Pll3 pfd2. */
    ANADIG_PLL->SYS_PLL3_PFD |= ANADIG_PLL_SYS_PLL3_PFD_PFD2_DIV1_CLKGATE_MASK;

    /* Disable System Pll3 pfd3. */
    ANADIG_PLL->SYS_PLL3_PFD |= ANADIG_PLL_SYS_PLL3_PFD_PFD3_DIV1_CLKGATE_MASK;

    /* Bypass Audio Pll. */
    CLOCK_SetPllBypass(kCLOCK_PllAudio, true);

    /* DeInit Audio Pll. */
    CLOCK_DeinitAudioPll();

    /* Bypass Video Pll. */
    CLOCK_SetPllBypass(kCLOCK_PllVideo, true);

    /* DeInit Video Pll. */
    CLOCK_DeinitVideoPll();

    /* Module clock root configurations. */
    /* Configure M7 using ARM_PLL_CLK */
    rootCfg.mux = kCLOCK_M7_ClockRoot_MuxArmPllOut;
    rootCfg.div = 2;
    CLOCK_SetRootClock(kCLOCK_Root_M7, &rootCfg);

    CLOCK_PowerOffRootClock(kCLOCK_Root_M4);

    /* Configure BUS using SYS_PLL3_CLK */
    rootCfg.mux = kCLOCK_BUS_ClockRoot_MuxSysPll3Out;
    rootCfg.div = 2;
    CLOCK_SetRootClock(kCLOCK_Root_Bus, &rootCfg);

    /* Configure BUS_LPSR using SYS_PLL3_CLK */
    rootCfg.mux = kCLOCK_BUS_LPSR_ClockRoot_MuxSysPll3Out;
    rootCfg.div = 3;
    CLOCK_SetRootClock(kCLOCK_Root_Bus_Lpsr, &rootCfg);

    /* Configure CSSYS using SYS_PLL2_CLK */
    rootCfg.mux = kCLOCK_CSSYS_ClockRoot_MuxSysPll2Out;
    rootCfg.div = 4;
    CLOCK_SetRootClock(kCLOCK_Root_Cssys, &rootCfg);

    /* Configure CSTRACE using OSC_24M */
    rootCfg.mux = kCLOCK_CSTRACE_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Cstrace, &rootCfg);

    CLOCK_PowerOffRootClock(kCLOCK_Root_M4_Systick);

    /* Configure M7_SYSTICK using OSC_RC_400M */
    rootCfg.mux = kCLOCK_M7_SYSTICK_ClockRoot_MuxOscRc400M;
    rootCfg.div = 8;
    CLOCK_SetRootClock(kCLOCK_Root_M7_Systick, &rootCfg);

    /* Configure ADC1 using OSC_24M */
    rootCfg.mux = kCLOCK_ADC1_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Adc1, &rootCfg);

    /* Configure ADC2 using OSC_24M */
    rootCfg.mux = kCLOCK_ADC2_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Adc2, &rootCfg);

    /* Configure ACMP using OSC_24M */
    rootCfg.mux = kCLOCK_ACMP_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Acmp, &rootCfg);

    /* Configure FLEXIO1 using OSC_24M */
    rootCfg.mux = kCLOCK_FLEXIO1_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Flexio1, &rootCfg);

    /* Configure FLEXIO2 using OSC_24M */
    rootCfg.mux = kCLOCK_FLEXIO2_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Flexio2, &rootCfg);

    /* Configure GPT1 using OSC_24M */
    rootCfg.mux = kCLOCK_GPT1_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Gpt1, &rootCfg);

    /* Configure GPT2 using OSC_24M */
    rootCfg.mux = kCLOCK_GPT2_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Gpt2, &rootCfg);

    /* Configure GPT3 using OSC_24M */
    rootCfg.mux = kCLOCK_GPT3_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Gpt3, &rootCfg);

    /* Configure GPT4 using OSC_24M */
    rootCfg.mux = kCLOCK_GPT4_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Gpt4, &rootCfg);

    /* Configure GPT5 using OSC_24M */
    rootCfg.mux = kCLOCK_GPT5_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Gpt5, &rootCfg);

    /* Configure GPT6 using OSC_RC_400M */
    rootCfg.mux = kCLOCK_GPT6_ClockRoot_MuxOscRc400M;
    rootCfg.div = 6;
    CLOCK_SetRootClock(kCLOCK_Root_Gpt6, &rootCfg);

    /* Configure FLEXSPI1 using OSC_24M */
#if !(defined(XIP_EXTERNAL_FLASH) && (XIP_EXTERNAL_FLASH == 1) || defined(FLEXSPI_IN_USE))
    rootCfg.mux = kCLOCK_FLEXSPI1_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Flexspi1, &rootCfg);
#endif

    /* Configure FLEXSPI2 using SYS_PLL2_PFD2_CLK */
    rootCfg.mux = kCLOCK_FLEXSPI2_ClockRoot_MuxSysPll2Pfd2;
    rootCfg.div = 3;
    CLOCK_SetRootClock(kCLOCK_Root_Flexspi2, &rootCfg);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Can1);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Can2);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Can3);

    /* Configure LPUART1 using OSC_RC_400M */
    rootCfg.mux = kCLOCK_LPUART1_ClockRoot_MuxOscRc400M;
    rootCfg.div = 6;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart1, &rootCfg);

    /* Configure LPUART2 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART2_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart2, &rootCfg);

    /* Configure LPUART3 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART3_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart3, &rootCfg);

    /* Configure LPUART4 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART4_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart4, &rootCfg);

    /* Configure LPUART5 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART5_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart5, &rootCfg);

    /* Configure LPUART6 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART6_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart6, &rootCfg);

    /* Configure LPUART7 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART7_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart7, &rootCfg);

    /* Configure LPUART8 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART8_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart8, &rootCfg);

    /* Configure LPUART9 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART9_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart9, &rootCfg);

    /* Configure LPUART10 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART10_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart10, &rootCfg);

    /* Configure LPUART11 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART11_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart11, &rootCfg);

    /* Configure LPUART12 using OSC_24M */
    rootCfg.mux = kCLOCK_LPUART12_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpuart12, &rootCfg);

    /* Configure LPI2C1 using OSC_24M */
    rootCfg.mux = kCLOCK_LPI2C1_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpi2c1, &rootCfg);

    /* Configure LPI2C2 using OSC_24M */
    rootCfg.mux = kCLOCK_LPI2C2_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpi2c2, &rootCfg);

    /* Configure LPI2C3 using OSC_24M */
    rootCfg.mux = kCLOCK_LPI2C3_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpi2c3, &rootCfg);

    /* Configure LPI2C4 using OSC_24M */
    rootCfg.mux = kCLOCK_LPI2C4_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpi2c4, &rootCfg);

    /* Configure LPI2C5 using OSC_24M */
    rootCfg.mux = kCLOCK_LPI2C5_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpi2c5, &rootCfg);

    /* Configure LPI2C6 using OSC_24M */
    rootCfg.mux = kCLOCK_LPI2C6_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpi2c6, &rootCfg);

    /* Configure LPSPI1 using SYS_PLL2_PFD3_CLK */
    rootCfg.mux = kCLOCK_LPSPI1_ClockRoot_MuxSysPll2Pfd3;
    rootCfg.div = 11;
    CLOCK_SetRootClock(kCLOCK_Root_Lpspi1, &rootCfg);

    /* Configure LPSPI2 using SYS_PLL2_PFD3_CLK */
    rootCfg.mux = kCLOCK_LPSPI2_ClockRoot_MuxSysPll2Pfd3;
    rootCfg.div = 11;
    CLOCK_SetRootClock(kCLOCK_Root_Lpspi2, &rootCfg);

    /* Configure LPSPI3 using SYS_PLL2_PFD3_CLK */
    rootCfg.mux = kCLOCK_LPSPI3_ClockRoot_MuxSysPll2Pfd3;
    rootCfg.div = 11;
    CLOCK_SetRootClock(kCLOCK_Root_Lpspi3, &rootCfg);

    /* Configure LPSPI4 using SYS_PLL2_PFD3_CLK */
    rootCfg.mux = kCLOCK_LPSPI4_ClockRoot_MuxSysPll2Pfd3;
    rootCfg.div = 11;
    CLOCK_SetRootClock(kCLOCK_Root_Lpspi4, &rootCfg);

    /* Configure LPSPI5 using OSC_24M */
    rootCfg.mux = kCLOCK_LPSPI5_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpspi5, &rootCfg);

    /* Configure LPSPI6 using OSC_24M */
    rootCfg.mux = kCLOCK_LPSPI6_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Lpspi6, &rootCfg);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Emv1);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Emv2);

    /* Configure ENET1 using OSC_24M */
    rootCfg.mux = kCLOCK_ENET1_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Enet1, &rootCfg);

    /* Configure ENET2 using SYS_PLL1_DIV2_CLK */
    rootCfg.mux = kCLOCK_ENET2_ClockRoot_MuxSysPll1Div2;
    rootCfg.div = 4;
    CLOCK_SetRootClock(kCLOCK_Root_Enet2, &rootCfg);

    /* Configure ENET_QOS using OSC_24M */
    rootCfg.mux = kCLOCK_ENET_QOS_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Enet_Qos, &rootCfg);

    /* Configure ENET_25M using OSC_24M */
    rootCfg.mux = kCLOCK_ENET_25M_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Enet_25m, &rootCfg);

    /* Configure ENET_TIMER1 using OSC_24M */
    rootCfg.mux = kCLOCK_ENET_TIMER1_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Enet_Timer1, &rootCfg);

    /* Configure ENET_TIMER2 using OSC_24M */
    rootCfg.mux = kCLOCK_ENET_TIMER2_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Enet_Timer2, &rootCfg);

    /* Configure ENET_TIMER3 using OSC_24M */
    rootCfg.mux = kCLOCK_ENET_TIMER3_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Enet_Timer3, &rootCfg);

    /* Configure USDHC1 using OSC_24M */
    rootCfg.mux = kCLOCK_USDHC1_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Usdhc1, &rootCfg);

    /* Configure USDHC2 using OSC_24M */
    rootCfg.mux = kCLOCK_USDHC2_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Usdhc2, &rootCfg);

    /* Configure ASRC using OSC_24M */
    rootCfg.mux = kCLOCK_ASRC_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Asrc, &rootCfg);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Mqs);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Mic);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Spdif);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Sai1);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Sai2);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Sai3);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Sai4);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Gc355);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Lcdif);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Lcdifv2);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Mipi_Ref);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Mipi_Esc);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Csi2);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Csi2_Esc);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Csi2_Ui);

    CLOCK_PowerOffRootClock(kCLOCK_Root_Csi);

    /* Configure CKO1 using OSC_24M */
    rootCfg.mux = kCLOCK_CKO1_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Cko1, &rootCfg);

    /* Configure CKO2 using OSC_24M */
    rootCfg.mux = kCLOCK_CKO2_ClockRoot_MuxOsc24MOut;
    rootCfg.div = 1;
    CLOCK_SetRootClock(kCLOCK_Root_Cko2, &rootCfg);

    /* Set SAI1 MCLK1 clock source. */
    IOMUXC_SetSaiMClkClockSource(IOMUXC_GPR, kIOMUXC_GPR_SAI1MClk1Sel, 0);
    /* Set SAI1 MCLK2 clock source. */
    IOMUXC_SetSaiMClkClockSource(IOMUXC_GPR, kIOMUXC_GPR_SAI1MClk2Sel, 3);
    /* Set SAI1 MCLK3 clock source. */
    IOMUXC_SetSaiMClkClockSource(IOMUXC_GPR, kIOMUXC_GPR_SAI1MClk3Sel, 0);
    /* Set SAI2 MCLK3 clock source. */
    IOMUXC_SetSaiMClkClockSource(IOMUXC_GPR, kIOMUXC_GPR_SAI2MClk3Sel, 0);
    /* Set SAI3 MCLK3 clock source. */
    IOMUXC_SetSaiMClkClockSource(IOMUXC_GPR, kIOMUXC_GPR_SAI3MClk3Sel, 0);

    /* Set MQS configuration. */
    IOMUXC_MQSConfig(IOMUXC_GPR,kIOMUXC_MqsPwmOverSampleRate32, 0);
    /* Set ENET Ref clock source. */
    IOMUXC_GPR->GPR4 &= ~IOMUXC_GPR_GPR4_ENET_REF_CLK_DIR_MASK;
    /* Set ENET_1G Tx clock source. */
    IOMUXC_GPR->GPR5 = ((IOMUXC_GPR->GPR5 & ~IOMUXC_GPR_GPR5_ENET1G_TX_CLK_SEL_MASK) | IOMUXC_GPR_GPR5_ENET1G_RGMII_EN_MASK);
    /* Set ENET_1G Ref clock source. */
    IOMUXC_GPR->GPR5 &= ~IOMUXC_GPR_GPR5_ENET1G_REF_CLK_DIR_MASK;
    /* Set ENET_QOS Tx clock source. */
    IOMUXC_GPR->GPR6 &= ~IOMUXC_GPR_GPR6_ENET_QOS_RGMII_EN_MASK;
    /* Set ENET_QOS Ref clock source. */
    IOMUXC_GPR->GPR6 &= ~IOMUXC_GPR_GPR6_ENET_QOS_REF_CLK_DIR_MASK;
    /* Set GPT1 High frequency reference clock source. */
    IOMUXC_GPR->GPR22 &= ~IOMUXC_GPR_GPR22_REF_1M_CLK_GPT1_MASK;
    /* Set GPT2 High frequency reference clock source. */
    IOMUXC_GPR->GPR23 &= ~IOMUXC_GPR_GPR23_REF_1M_CLK_GPT2_MASK;
    /* Set GPT3 High frequency reference clock source. */
    IOMUXC_GPR->GPR24 &= ~IOMUXC_GPR_GPR24_REF_1M_CLK_GPT3_MASK;
    /* Set GPT4 High frequency reference clock source. */
    IOMUXC_GPR->GPR25 &= ~IOMUXC_GPR_GPR25_REF_1M_CLK_GPT4_MASK;
    /* Set GPT5 High frequency reference clock source. */
    IOMUXC_GPR->GPR26 &= ~IOMUXC_GPR_GPR26_REF_1M_CLK_GPT5_MASK;
    /* Set GPT6 High frequency reference clock source. */
    IOMUXC_GPR->GPR27 &= ~IOMUXC_GPR_GPR27_REF_1M_CLK_GPT6_MASK;

#if __CORTEX_M == 7
    SystemCoreClock = CLOCK_GetRootClockFreq(kCLOCK_Root_M7);
#else
    SystemCoreClock = CLOCK_GetRootClockFreq(kCLOCK_Root_M4);
#endif
}

 

 

 

you can see that M4 is OFF, so if we change the code in this way

//    CLOCK_PowerOffRootClock(kCLOCK_Root_M4);         old code

 

    /* Configure M4 using OSC_RC_400M */                               enable clock CM4

     rootCfg.mux = kCLOCK_M4_ClockRoot_MuxOscRc400M;

     rootCfg.div = 1;

     CLOCK_SetRootClock(kCLOCK_Root_M4, &rootCfg);

the M4 clock ON solves the issue.

 

Best regards

0 项奖励
回复

1,652 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Although the RT1171 does not have a second core it still has the M4 Root clock which is used for source for other modules such as JTAG. So the suggestion is not to power-off the Root M4 but do not initialize it.

Best regards,
Omar

0 项奖励
回复

1,628 次查看
Nexus76
Contributor II

Hi Omar,

so you suggest to do this

 

 
 

conf.jpg

...so without this code

 

/* Configure M4 using OSC_RC_400M */
rootCfg.mux = kCLOCK_M4_ClockRoot_MuxOscRc400M;
rootCfg.div = 1;
CLOCK_SetRootClock(kCLOCK_Root_M4, &rootCfg);

 

is it corret ?

I'd like to understand that the M4 root must be ON because these pheripericals are used by M7 ?

 

pheriperical.png

Best regards

0 项奖励
回复

1,476 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Correct, it is suggested to leave the root enabled as there are other modules that feed from that root such the ones on the image as well as JTAG.

Omar_Anguiano_0-1741904011463.png

Best regards,
Omar

0 项奖励
回复