Converting Bin file generated from IAR into Hex file for Flash Magic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Converting Bin file generated from IAR into Hex file for Flash Magic

4,100件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by milind.mishra on Wed May 13 23:06:17 MST 2015
Hi,

I have to flash a firmware on my LPC43xx based board. I am using IAR IDE and can generate a bin file. How do I convert it to a hex file which can be flashed on the SPIFI flash on the board?

Can anyone tell the steps that I need to follow?

Regards,
Milind
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,563件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Thu May 14 00:51:43 MST 2015
IAR will generate the hex file directly. Search for "iar create hex"
0 件の賞賛
返信

3,563件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by milind.mishra on Thu May 14 00:06:35 MST 2015
It tells about the generic way which I am able to do. What I need is a method to generate a hex file which can be flashed on the SPIFI NOR from  the bin file generated by IAR.
0 件の賞賛
返信

3,563件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mysepp on Wed May 13 23:20:53 MST 2015
Have a look at this link (on page 7):

http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=swru038&fileType=pdf

This document is not for NXP controller, but they use IAR IDE. Perhaps the same setting is available in your IAR IDE?
0 件の賞賛
返信