Convert to gray

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Convert to gray

1,197 Views
thomasjohansen
Contributor I

Hi

I'm using the LPC1788 with a 16 bpp Color TFT display.

Is it somehow possible to get the LCD controller to convert the colors to gray scale?

Or do I need to convert the colors elsewhere. GUI or framebuffer?

Thomas

Labels (1)
0 Kudos
Reply
1 Reply

1,155 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Thomas,

 

LPC178x MCUs include gray scale algorithms for STN displays only.  This provides 15 gray scales for monochrome displays.

 

Unfortunately, we do not have any gray scaler for TFT displays. In order to convert the colors you may use an external IC.

 

Sorry for the inconvenience this may cause you.

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply