Conversion frecuency in ADC burst mode (LPC802)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Conversion frecuency in ADC burst mode (LPC802)

ソリューションへジャンプ
1,208件の閲覧回数
asier
Contributor III

Hi,

Is it possible to do conversions slower in ADC burst mode ? 

I'm doing 1 channel conversion in SEQA burst mode. Interrupt with entire sequence is enabled. 

My issue is that the interrupt callback is happening every 12us, so as soon as code leaves interrupt callback it is called again and code in main is almost blocked.

Is there any way to slow down the conversión rate ? 

Thanks in advance,

Asier.

0 件の賞賛
返信
1 解決策
1,190件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi asier 

The ADC controller uses the system clock as a bus clock. We can only reduce ADC conversion time by reducing ADC working clock. No option to slow down burst conversion rate only.

ZhangJennie_0-1647416784836.png

Have a nice day

Jun Zhang

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,191件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi asier 

The ADC controller uses the system clock as a bus clock. We can only reduce ADC conversion time by reducing ADC working clock. No option to slow down burst conversion rate only.

ZhangJennie_0-1647416784836.png

Have a nice day

Jun Zhang

 

0 件の賞賛
返信