Connecting LPC4357 to OLED on a 6800/8080 parallel bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connecting LPC4357 to OLED on a 6800/8080 parallel bus

1,155件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akrylik on Thu Jul 16 03:12:07 MST 2015
What is the recommended peripheral to use when connecting to an OLED (or any) display that uses a 8-bit 6800/8080 parallel bus?  My initial research into the subject seems to imply that you should use the EMC+DMA.  However I'm already using the EMC for external SDRAM.  Is it possible to use the LCD controller for this purpose?  How about the SGPIO+DMA?

So the 3 options that I've identified:

EMC+DMA
-  Will there be bus contention with external SDRAM?

LCD Controller?
- The LPC43xx manual doesn't mention the 6800/8080 parallel bus at all.

SGPIO+DMA


Any advise, reference circuits/code would be greatly appreciated.


Thank you.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)