Connect usb printer to lpc54018

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connect usb printer to lpc54018

1,791件の閲覧回数
oscarniño
Contributor III

Hi

I'm working with lpc54018, In a new project we will to connect a 7 in display, a usb printer, ethernet, serial comunication, etc.  my question is: Is posible to connect it an usb printer? If yes, is there any source available to do it? Thank you so much.

Best regards

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,708件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Oscar,

Regarding your question, I have checked out SDK package, we support the USB printer class, we have developed the USB printer driver.

Pls download SDK package from the link:

Welcome | MCUXpresso SDK Builder 

In the SDK package, we have the USB device printer example as following.

I attach the readme file for the USB printer example

Hope it can help you

BR

XiangJun Rong

pastedImage_2.png