Connect bits streams at 13Mhz to GPIOs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connect bits streams at 13Mhz to GPIOs

1,737 次查看
michcor
Contributor I

Hello,
I have a board which have 8 x bit streams. Each bit stream has its own associated bit clock. So I have: 8 x 2pins (one for the bit stream, one for its associated bit clock). Each bit clock is at 13mhz.

I would like to connect these streams to GPIOs pins of a single Cortex-M MCU for further processing. Which LPC should I use?


Thx,
Michel

0 项奖励
回复
3 回复数

1,640 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Michel,

Are the bit clocks going to be synchronized? or you are going to sample each stream bit separately based on its clock? I think the LPC43xx family of high performance MCUs could achieve the sample frequency you need:

LPC4300 Series: High Performance Microcontrollers (MCUs) based on ARM® Cortex®-M4/M0 Cores|NXP 

Please notice that processing an interrupt takes time, it takes you 12 cycles to get into the ISR so whatever the GPIO pad is physically able to do, the determining factor is the time you spend on going into the ISR and run the ISR.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复

1,640 次查看
michcor
Contributor I

Hello Carlos,

hank you for your response.

Bit clocks are not synchronized and I need to sample each stream bit separately based on its clock.

Does the LPC4300 is able to handle these streams in parallel?

thx

Regards

Michel

0 项奖励
回复

1,640 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Michel,

 

This will depend on which other tasks are going to be executed in your program and the time it will take you to process the sampled data.

Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复