Connect LPC1114FN28 to LPC-Link 2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connect LPC1114FN28 to LPC-Link 2

1,850件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by joosts on Sat Apr 05 11:09:28 MST 2014
Hi,

I've been experimenting with the excellent LPC1114FN28 (DIP)chip on breadboard-projects, programming the chip using ISP.
I would like to be able to connect my LPC-Link 2 board to the LPC1114FN28 chip, so I can use single wire debug.

Could anyone tell me which connector/pins of the LPC-Link 2 board should be connected to which pins of the LPC1114FN28, since I am unable to find a clear description of the pins of the LPC-Link 2 board...

Thanks in advance,
Joost
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,796件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by joosts on Sat Apr 05 12:03:06 MST 2014
Thanks a lot!
0 件の賞賛
返信

1,796件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Sat Apr 05 11:59:08 MST 2014

Quote: joosts
Am I correct to understand that I could use the J6 connector of LPC Link 2?



Yes  :)


Quote: joosts
Could you please verify if I understood correctly that I would need to connect:

LPC Link 2 connector J6 pin 2 (JTAG_TMS_SWDIO) to pin 12 of LPC1114FN28
LPC Link 2 connector J6 pin 3 (JTAG_TMS_SWCLK) to pin 3 of LPC1114FN28
LPC Link 2 connector J6 pin 6 (JTAG_RESET) to pin 23 of LPC1114FN28
LPC Link 2 connector J6 pin 8 (GND) to pin 22 of LPC1114FN28



Right.

Don't forget to pull-up Reset and ISP and your board should work...
0 件の賞賛
返信

1,796件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by joosts on Sat Apr 05 11:48:54 MST 2014
Thanks for your swift response.

Am I correct to understand that I could use the J6 connector of LPC Link 2?

Could you please verify if I understood correctly that I would need to connect:

LPC Link 2 connector J6 pin 2 (JTAG_TMS_SWDIO) to pin 12 of LPC1114FN28
LPC Link 2 connector J6 pin 3 (JTAG_TMS_SWCLK) to pin 3 of LPC1114FN28
LPC Link 2 connector J6 pin 6 (JTAG_RESET) to pin 23 of LPC1114FN28
LPC Link 2 connector J6 pin 8 (GND) to pin 22 of LPC1114FN28

(I have consulted sheet 5 of the LPC Link2 schematic at http://www.embeddedartists.com/products/lpcxpresso/lpclink2.php and page 26-28 of the LPC111x datasheet at http://www.nxp.com/documents/data_sheet/LPC111X.pdf).

Thanks in advance!
Joost

0 件の賞賛
返信

1,796件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Sat Apr 05 11:24:49 MST 2014
Just use a simple 4-wire connection:

http://www.lpcware.com/content/forum/lpc15xx-minimal-swd

Link2 schematic:

http://www.embeddedartists.com/products/lpcxpresso/lpclink2.php
0 件の賞賛
返信