Confusing for Peripherials config for LPC55S16 in sample code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Confusing for Peripherials config for LPC55S16 in sample code

1,033件の閲覧回数
ygao
Contributor I

Hi,

For a I2C setting to use Flexcomm4, it needs to config clock on Clocks config for FXCOMCLK4, and config Flexcomm4 pins to be I2C in Peripherials config, right?

However, in LPC55S16 sample code, e.g., lpcxpresso55s16_multi_peripherals_test, non clock is configured in Clocks config for Flexcomm4, and non I2C is configured in Peripherals config. Why?

Is it because all the code are input manually instead of generating by configs?

Thanks,

Winston

ラベル(1)
0 件の賞賛
返信
1 返信

1,020件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ygao 

Yes, some of examples not use Configure tool to config. The code is  input manually .

 

BR

Alice

0 件の賞賛
返信