Configure SCTimer with PWM Mode and Interrupt using Config Tools on LPC546xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configure SCTimer with PWM Mode and Interrupt using Config Tools on LPC546xx

1,417件の閲覧回数
robsongordo2017
Contributor I
Configure SCTimer with PWM Mode and interrupt with pinout togle event using Config Tools 
on LPC546xx. The PWM signal is generated perfectly but the interruption does not occur 
or the vector does not point to the routine. Note below the code generated after 
compiling config tools.
/***********************************************************************************************************************
 * SCTimer_0 initialization code
 **********************************************************************************************************************/
/* clang-format off */
/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
instance:
- name: 'SCTimer_0'
- type: 'sctimer'
- mode: 'basic'
- type_id: 'sctimer_11116c58643bd290f0e74db0acbc9466'
- functional_group: 'BOARD_InitPeripherals'
- peripheral: 'SCT0'
- config_sets:
  - main:
    - config:
      - clockMode: 'kSCTIMER_System_ClockMode'
      - clockSource: 'SynchronousFunctionClock'
      - clockSourceFreq: 'GetFreq'
      - SCTInputClockSourceFreq: 'custom:0'
      - clockSelect: 'kSCTIMER_Clock_On_Rise_Input_0'
      - enableCounterUnify: 'true'
      - enableBidirection_l: 'true'
      - enableBidirection_h: 'false'
      - prescale_l: '1'
      - prescale_h: '1'
      - outInitState: 'SCTIMER_OUTPUT_7_MASK'
    - enableIRQ: 'true'
    - interrupt:
      - IRQn: 'SCT0_IRQn'
      - enable_priority: 'false'
      - enable_custom_name: 'false'
    - enableLTimer: 'true'
    - enableHTimer: 'false'
    - pwms:
      - 0:
        - output: 'kSCTIMER_Out_7'
        - level: 'kSCTIMER_HighTrue'
        - dutyCyclePercent: '75'
    - pwmMode: 'kSCTIMER_CenterAlignedPwm'
    - pwmFrequency: '20000'
    - events:
      - 0:
        - type: 'kSCTIMER_OutputRiseEvent'
        - output: 'kSCTIMER_Out_7'
        - actions: []
    - states:
      - 0:
        - pwms: 'pwm0'
        - events: 'event0'
 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/
/* clang-format on */
const sctimer_config_t SCTimer_0_initConfig = {
  .enableCounterUnify = true,
  .clockMode = kSCTIMER_System_ClockMode,
  .clockSelect = kSCTIMER_Clock_On_Rise_Input_0,
  .enableBidirection_l = true,
  .enableBidirection_h = false,
  .prescale_l = 0,
  .prescale_h = 0,
  .outInitState = SCTIMER_OUTPUT_7_MASK
};
const sctimer_pwm_signal_param_t SCTimer_0_pwmSignalsConfig[1] = {
  {
    .output = kSCTIMER_Out_7,
    .level = kSCTIMER_HighTrue,
    .dutyCyclePercent = 75
  }
};
uint32_t SCTimer_0_pwmEvent[1];
uint32_t SCTimer_0_event[1];

void SCTimer_0_init(void) {
  SCTIMER_Init(SCTIMER_0_PERIPHERAL, &SCTimer_0_initConfig);
  /* Initialization of state 0 */
  SCTIMER_SetupPwm(SCTIMER_0_PERIPHERAL, &SCTimer_0_pwmSignalsConfig[0], kSCTIMER_CenterAlignedPwm, 20000U, SCTIMER_0_CLOCK_FREQ, &SCTimer_0_pwmEvent[0]);
  SCTIMER_CreateAndScheduleEvent(SCTIMER_0_PERIPHERAL, kSCTIMER_OutputRiseEvent, 0, kSCTIMER_Out_7, kSCTIMER_Counter_L, &SCTimer_0_event[0]);
  /* Enable interrupt SCT0_IRQn request in the NVIC */
  EnableIRQ(SCTIMER_0_IRQN);
  SCTIMER_StartTimer(SCTIMER_0_PERIPHERAL, kSCTIMER_Counter_L);
}

... and ....

void EV_InterruptSCT0(void)
{  temp_timer++;    if(temp_timer & 0x0001) PIO_test_ON();  else PIO_test_OFF(); }
 
// Oscilloscope has no signal at PIO_test, but the pwm 20KHz at PIO_7, 
// duty 75% OK. The interruption does not happen

... and ....(main)

BOARD_InitPeripherals();
SCTIMER_SetCallback(SCT0,EV_InterruptSCT0,0);





0 件の賞賛
返信
1 返信

1,340件の閲覧回数
soledad
NXP Employee
NXP Employee

Please check the updates in the following thread:

https://community.nxp.com/thread/511273 

Regards

Soledad

0 件の賞賛
返信