Configuration of external SPI RAM as memory mapped access in LPC1778 microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuration of external SPI RAM as memory mapped access in LPC1778 microcontroller

908 Views
SomashekaraV
Contributor I

Hi all,

As part of our customized controller board(LPC1778 based), we have used external SPI interfaced RAM memory of 1 Mbit device. So it is possible to configure this memory to be used as extended memory to our controller. Is there any other mechanism to map it as another bank of memory.

Thanks,
Somashekara

0 Kudos
Reply
1 Reply

815 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The LPC1778 has spifi interface,in general,  if you connect the spi RAM to the spifi interface, you can allocate the spifi RAM to the address 0x2800_0000 to 0x28FF_FFFF, when the core access the above address, the spifi module can generate the spifi timing to access the spifi RAM.

Can you tell us the part number of the spi RAM so that we can have a check?

xiangjun_rong_1-1696747910176.png

 


Hope it is helpful.


BR

XiangJun Rong

 

 

 

0 Kudos
Reply