Config Tools Option for LPC4370

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Config Tools Option for LPC4370

1,360 次查看
mhpham23
Contributor I

Hi,

I am doing a project with the LPC4370 chip. I am wondering if either LPCXpresso or MCUXpresso has the config tools option for it. I have been trying to open up the config tools in MCUXpresso but it's not working since LPC4370 doesn't have SDK package.
If LPC4370 doesn't have the option for config tools at all, is there a chip that has the same capability of 80MHz data acquisition  that has the config tools option?

Thanks!

标签 (1)
0 项奖励
回复
1 回复

1,357 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Hoan,

Unfortunately, for LPC43xx, there is not configuration tools to configure the HSADC module of LPC4370. The MCUXpresso tools includes configuration tools, but the tools does not support LPC4370, the LPC4370 is a bit old.

This is an unofficial code for the HSADC plus DMA, pls refer to it.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复