Config Tools Option for LPC4370

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Config Tools Option for LPC4370

1,371件の閲覧回数
mhpham23
Contributor I

Hi,

I am doing a project with the LPC4370 chip. I am wondering if either LPCXpresso or MCUXpresso has the config tools option for it. I have been trying to open up the config tools in MCUXpresso but it's not working since LPC4370 doesn't have SDK package.
If LPC4370 doesn't have the option for config tools at all, is there a chip that has the same capability of 80MHz data acquisition  that has the config tools option?

Thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

1,368件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Hoan,

Unfortunately, for LPC43xx, there is not configuration tools to configure the HSADC module of LPC4370. The MCUXpresso tools includes configuration tools, but the tools does not support LPC4370, the LPC4370 is a bit old.

This is an unofficial code for the HSADC plus DMA, pls refer to it.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信