Communication between Lpc board and Dongle using FTDI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Communication between Lpc board and Dongle using FTDI

2,082 次查看
aws1995
Contributor I

Hello,
Please, I want to ask if an LPC board can Communicate with Dongle OM15080-K32W using FTDI or other types of Dongles using FTDI?

0 项奖励
回复
3 回复数

2,053 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Specifically, how are you planning to do the communication?
The MCU inside the dongle is acceded through UART and uses a USB to UART converter to make it possible. So using a device with a USB makes it possible to communicate with the dongle.

I looking forward to your reply. IF you have more questions do not hesitate to ask me.
Best regards,
Omar

0 项奖励
回复

2,031 次查看
aws1995
Contributor I

@Omar_Anguiano  Hallo and thanks very much for the answer , i have used k32 with lpcXpresso55s69 Board , i would like to send data from my pc to lpc board then to forward this data to the k32 and then to recieve data from anoher k32 dongle , but the  problem is that lpc board support only uart with cdc , but as iknow that k32 support only ftdi and lpc borad do not support ftdi and i can not till now find a solution for that ?

0 项奖励
回复

2,007 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
You can use the USB full speed from the LPC55s69 to connect with the K32W. I suggest you contact FTDI to check if some modifications are needed for the USB CDC of the LPC55s69. Since both devices use USB communication is possible.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 项奖励
回复