Clock error on custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clock error on custom board

ソリューションへジャンプ
2,103件の閲覧回数
englemon
Contributor II

I have been trying to get a custom board working over SWD using the link-2. When downloading code to the board I am getting an error and when stepping through the code the last line I get too before the error occurs is:

__STATIC_INLINE void Chip_Clock_SetMain_B_ClockSource(CHIP_SYSCON_MAIN_B_CLKSRC_T src)
{
LPC_SYSCON->MAINCLKSELB = (uint32_t) src;
}

in clock_5410x.h

After this a new tab pops up with 

No source available for "0x35dbeb88" 

The disassembly reads:

Failed to execute MI command:
-data-disassemble -s 903605152 -e 903605248 -- 3
Error message from debugger back end:
Cannot access memory at address 0x35dbeba0

I am using the LPC54101J512BD64QL

I am new to this an really need help.

Much thanks

0 件の賞賛
返信
1 解決策
1,964件の閲覧回数
englemon
Contributor II
0 件の賞賛
返信
2 返答(返信)
1,965件の閲覧回数
englemon
Contributor II
0 件の賞賛
返信
1,964件の閲覧回数
englemon
Contributor II

To add some info I am trying to run the basic LPCOpen project for the chip using LPCXpresso with no real changes to the code.

0 件の賞賛
返信