Chip Replacement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Chip Replacement

3,064 Views
HerrPhy
Contributor I

We are now using the LPC11U24FBD48/401 chipset for mass production. Just for a backup, may I ask that is there an alternative chip that can replace it but without changing the firmware.bin?

Thanks very much in advance.

0 Kudos
Reply
4 Replies

3,049 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, HerrPhy,

Pls download the data sheet of LPC11U2x from the link:

https://www.nxp.com/docs/en/data-sheet/LPC11U2X.pdf

 

Pls refer to the Fig 4, all the LPC11U22FBD48/301, LPC11U23FBD48/301,LPC11U24FBD48/301, LPC11U24FBD48/401 are pin to pin compatible, but only  the memory size are different.

 

xiangjun_rong_0-1598943823840.pngxiangjun_rong_0-1598943823840.png

 

BTW, this is the resource of the chip

xiangjun_rong_1-1598943928892.pngxiangjun_rong_1-1598943928892.png

Hope it can help you

BR

XiangJun Rong

 

 

0 Kudos
Reply

3,047 Views
HerrPhy
Contributor I

Thanks for the reply. Can I use other serial like 11U34FBD48/421 or 11U35FBD48/401 to replace the 11U24 serial chip? Are they also binary code compatible?

 

0 Kudos
Reply

3,010 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, HerrPhy,

I have compared the pin assignment for the 11U34FBD48/421, 11U35FBD48/401 and LPC11U24FBD48/401, I think the pin assignment are the same, pls check again yourself.

Regarding the "binary code compatible" question, I am sure all of them are binary code compatible, because they use the same core ARM Cortex-M0.

Hope it can help you

BR

XiangJun rong

0 Kudos
Reply

3,060 Views
HerrPhy
Contributor I

And also we don't wanna change the PCB so it should be a pin-2-pin compatible to LPC11U24FBD48/401

0 Kudos
Reply