Chip_Clock_IsUSBPLLLocked hangs when IRC is turned off

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Chip_Clock_IsUSBPLLLocked hangs when IRC is turned off

ソリューションへジャンプ
1,783件の閲覧回数
A_L
Contributor I

We use external 16MHz crystal oscillator for LPC11U68JBD48E clock:

unsigned int j;
SystemCoreClockUpdate();
Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_IOCON);

// start SYSOSC
Chip_IOCON_PinMuxSet(LPC_IOCON, 2, 0, (IOCON_FUNC1 | IOCON_MODE_INACT)); // PIO2_0 = XTALIN
Chip_IOCON_PinMuxSet(LPC_IOCON, 2, 1, (IOCON_FUNC1 | IOCON_MODE_INACT)); // PIO2_1 = XTALOUT
Chip_SYSCTL_PowerUp(SYSCTL_POWERDOWN_SYSOSC_PD);
Chip_Clock_SetPLLBypass(false, false);
for (j = 0; j < 0x400; ++j); // 500us delay is needed after SYSOSC is powered up

// MAINCLK = 64MHz, from PLL
Chip_Clock_SetMainClockSource(SYSCTL_MAINCLKSRC_IRC);
Chip_SYSCTL_PowerDown(SYSCTL_POWERDOWN_SYSPLL_PD);
Chip_Clock_SetSystemPLLSource(SYSCTL_PLLCLKSRC_MAINOSC);
Chip_Clock_SetupSystemPLL(3, 1); // FCLKIN = 16, FCLKOUT = 64, FCCO = 256MHz
Chip_SYSCTL_PowerUp(SYSCTL_POWERDOWN_SYSPLL_PD);
while (!Chip_Clock_IsSystemPLLLocked());
Chip_Clock_SetSysClockDiv(2); // system clock at 32Mhz
Chip_Clock_SetMainClockSource(SYSCTL_MAINCLKSRC_PLLOUT);
SystemCoreClockUpdate();

// so far so good, turning off IRC:
Chip_SYSCTL_PowerDown(SYSCTL_POWERDOWN_IRC_PD);
Chip_SYSCTL_PowerDown(SYSCTL_POWERDOWN_IRCOUT_PD);

// now lets try set up USB clock:
Chip_SYSCTL_PowerDown(SYSCTL_POWERDOWN_USBPLL_PD);
Chip_Clock_SetUSBPLLSource(SYSCTL_USBPLLCLKSRC_MAINOSC);
Chip_Clock_SetupUSBPLL(2, 1); // FCLKIN = 16, FCLKOUT = 48, FCCO = 192MHz
Chip_SYSCTL_PowerUp(SYSCTL_POWERDOWN_USBPLL_PD);
while (!Chip_Clock_IsUSBPLLLocked()); // hangs here indefinitely

// and this code is not reached ...
Chip_Clock_SetUSBClockSource(SYSCTL_USBCLKSRC_PLLOUT, 1);
Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_USB);
Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_USBRAM);
Chip_SYSCTL_PowerUp(SYSCTL_POWERDOWN_USBPAD_PD);

So, could USB PLL be used when IRC is turned off?

0 件の賞賛
返信
1 解決策
1,759件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Alexei,

It appears that you do not set up the USB PLL Clock source register, pls check.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1618191586471.pngxiangjun_rong_0-1618191586471.png

 

xiangjun_rong_1-1618191722703.pngxiangjun_rong_1-1618191722703.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,760件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Alexei,

It appears that you do not set up the USB PLL Clock source register, pls check.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1618191586471.pngxiangjun_rong_0-1618191586471.png

 

xiangjun_rong_1-1618191722703.pngxiangjun_rong_1-1618191722703.png

 

0 件の賞賛
返信
1,751件の閲覧回数
A_L
Contributor I

Hi, xiangjun_rong

Thanks, it appears I missed the line in manual: When switching clock sources, both clocks must be running.

When IRC is turned off after USB PLL setup, everything runs ok.

0 件の賞賛
返信