Changing baud rate of LPC 4370

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing baud rate of LPC 4370

1,887件の閲覧回数
vxs187
Contributor III

I don't know how to change the UART's baudrate for an LPC4370 microcontroller. I am using an example program from LPCExpresso to change the baudrate, from the board.c file. It has a function as follows:

Chip_UART_SetBaud(DEBUG_UART, 115200);

I have also included the function definition below:

uint32_t Chip_UART_SetBaud(LPC_USART_T *pUART, uint32_t baudrate)
{
uint32_t div, divh, divl, clkin;

/* Determine UART clock in rate without FDR */
clkin = Chip_Clock_GetRate(Chip_UART_GetClockIndex(pUART));
div = clkin / (baudrate * 16);

/* High and low halves of the divider */
divh = div / 256;
divl = div - (divh * 256);

Chip_UART_EnableDivisorAccess(pUART);
Chip_UART_SetDivisorLatches(pUART, divl, divh);
Chip_UART_DisableDivisorAccess(pUART);

/* Fractional FDR alreadt setup for 1 in UART init */

return clkin / div;
}

As seen, the baud rate is set by dividing the clkin by div. I am trying to achieve a baud rate higher than 115200, and it doesn't really work as it does for transferring data serially to an Arduino, as it does at 115200. I am new to using the microcontroller, any help would be greatly appreciated. 

Thanks!

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,753件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Visweshwar Srinivasan,

Please refer to the formula that is shown in the user guide section 40.6.12 to see which is the maximum baud rate you can reach depending on the peripheral clock. 

pastedImage_1.png

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信