Capture Qei position and send to usb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Capture Qei position and send to usb

944件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by AmirHejazi on Thu Jan 31 14:24:37 MST 2013
Hi
I want to draw graphs of position of 2-phased QEI versus time, using LPC1768. it is important to draw transient state between ON & OFF (to find step response!). An ENCLK_Int interrupt occurs at the every transition of the encoder and the firmware sends the timer value to USB.
I have written some codes. but FILE_Open, FILE_Write and FILE_Close are too slow to run in the QEI ISR, so i have send the data to a buffer and send them in batch.
but i don't know how to do it! :-|
how can i buffer the data? should i use an auxiliary register?
how can i detect that number of bytes written in QEITIME(or auxilary Buffer) is 512?
should i pend the interrupt to send the data(buffer) to USB? (cause the usb functions are too slow)



Best Regards 
Amir
ラベル(1)
0 件の賞賛
返信
0 返答(返信)