Capacitances for external RTC crystal in LPC4088

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Capacitances for external RTC crystal in LPC4088

跳至解决方案
3,737 次查看
kruftun
Contributor I

Could you recommend capacitances for external RTC crystal in LPC4088?

There is app note for it?

标签 (1)
0 项奖励
回复
1 解答
3,718 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Roman,

I think that it is okay to use 12.5pF capacitors, the capacitor value takes effect on the crystal clock frequency slightly. But there is not a formula to calculate the capacitor effect, you have to use a frequency meter to get the actual clock frequency.

Pls refer to the application note,it discusses the capacitor effect on the crystal clock frequency with experiment.

https://www.nxp.com.cn/docs/en/application-note/AN13057.pdf

Hope it can help you

BR

XiangJun Rong

 

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,732 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Roman,

I think you can refer to the design of LPC43xx, the two capacitors value of RTC are 18pF, you can use the 18pF capacitors.

Hope it can help you

BR

Xiangjun Rong

 

 

 

xiangjun_rong_0-1614839819592.pngxiangjun_rong_0-1614839819592.png

 

0 项奖励
回复
3,723 次查看
kruftun
Contributor I

Hi,
Thank you for answer. For example if crystal 32.768kHz with load capacitance 12.5 pF that 18pF capacitors will be right choice? May be there is some equation for capacitors calc?

0 项奖励
回复
3,719 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Roman,

I think that it is okay to use 12.5pF capacitors, the capacitor value takes effect on the crystal clock frequency slightly. But there is not a formula to calculate the capacitor effect, you have to use a frequency meter to get the actual clock frequency.

Pls refer to the application note,it discusses the capacitor effect on the crystal clock frequency with experiment.

https://www.nxp.com.cn/docs/en/application-note/AN13057.pdf

Hope it can help you

BR

XiangJun Rong

 

 

0 项奖励
回复